Can't find the X3 crystal recommended by ST from any supplier, nor can I find an equivalent that is in stock from any supplier.
Hi,
I have a STMF32446ZE board and require an external crystal that isn't using the STLINK crystal.
For x3 ST recommend the following: NX3225GD-8.000MEXS00A-CG04874
The specs of this crystal are:
Frequency Stability ±50ppm
Frequency Tolerance ±20ppm
Load Capacitance 8pF
Operating Temperature -40°C ~ 85°C
Mounting Type Surface Mount
Size / Dimension 0.126" L x 0.098" W (3.20mm x 2.50mm)
Frequency 8 MHz
ESR (Equivalent Series Resistance) 500 Ohms
Does anyone know of a crystal that can be used?
Thanks in advance, much appreciated!