STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

migration from keil to stm32cubemx ide

I am trying to migrate the keil project into stm32cube ide. startup file is generating errors. if I add the object files of keil project main.o, stm32f1xx_hal_msp.c and stm32f1xx_it.c along with the startup file(startup_stmf105rbtx.s generated from S...

KSag by Associate II
  • 1177 Views
  • 1 replies
  • 0 kudos

Resolved! What is the proper method to re-initialize SD card interface to support removal/reinsertion of SD card?

My SD card interface (using SDMMC1) stops working after the SD card has been removed/re-inserted.I have tried un-mounting using f_mount(0, &SDPath, 0) and then re-mounting with no success.As a test, I executed the following for each transaction:f_mou...

How to trigger clock and NCS of QSPI in STM32H7xx

Hi, i try to using QSPI in STM32H743( the STM32H743_Nucleo ) to received data, the programming IDE is STM32CubeIDE, and i used it to generated and assign pin and parameter. The clock and NCS pin is probed to oscilloscope, the code is as followed, whe...

cchan.21 by Associate II
  • 1579 Views
  • 1 replies
  • 0 kudos

STM32L152RET6 bank 1 and bank 2 switching:

Good day,I need some advise with switching banks on the STM32L152.Here's what I currently do:Flash a new, blank MCU and boot from bank 1.BOOT0 is externally pulled LOW. BOOT1 is being used otherwise.Load firmware starting at address 0x08040000 (start...

0693W00000HnaBGQAZ.png
HMull.1 by Associate II
  • 1662 Views
  • 2 replies
  • 0 kudos

How to use IDB05A1 in low power mode

i am using IDB05A1 and STM32F401RE MCU, X-CUBE-BLE1. i am trying to use IDB05A1 in low power mode. When the data is available MCU wake up from low power mode.@Sebastien DENOUAL​ @Community member​ @Peter BENSCH​ @Andrei MENGHIA​ 

HAL_QSPI_COMMAND locks up the QSPI FLASH

Dear All,I'm using STM32H757I-EVAL board. My stm32 cube ide version is 1.7.0.I'm trying the basic operation of reading the manufacture ID of the QSPI Flash.Below is the initialization code, which I have configured using STM32CubeMX.static void MX_QUA...

Aarra.1 by Senior
  • 2765 Views
  • 6 replies
  • 0 kudos