STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32U585QI SPI Issue

Hi,I have successfully configured the SPI1 with following parameters and trying to transfer a single byte but it is being timed-out in HAL_SPI_Transmit as EOT is not being set.Init.Mode = SPI_MODE_MASTER;Init.Direction = SPI_DIRECTION_2LINES;Init.Dat...

Ramin1 by Associate II
  • 2655 Views
  • 3 replies
  • 0 kudos

I need urgent help on STM32L071 RTC power consumption. when we enable standby mode, without RTC, the current from battery is <1uA . when we enable standby mode, WITH RTC, the current from battery is ~200 uA ? Which is too high to sustain

I need urgent help on STM32L071 RTC power consumption. when we enable standby mode, without RTC, the current from battery is <1uA. when we enable standby mode, WITH RTC, the current from battery is ~200 uA ? Which is too high to sustain

STM32F412 TIM3 16 bit or 32 bit ?

The reference manual (RM0402, DocID028087 Rev 7, Fig 4) shows TIM3 as a 32 bit timer. However, the in the description in Section 17.2, TIM3 and TIM4 are described as 16 bit timers.Is this a mistake in Figure 4 ?Thanks 

0693W00000HoK8rQAF.jpg 0693W00000HoK8wQAF.jpg
gahelton1 by Associate III
  • 1804 Views
  • 2 replies
  • 1 kudos

SDRAM HAL_SDRAM_WRITE_32b function not working for stm32H7.

Hello,I'm using STM32H757i-EVAL board and trying to store some data in the onboard SDRAM using stm32cubeide (1.7.0).Below is my initialization for SDRAMvoid MX_FMC_Init(void) {   /* USER CODE BEGIN FMC_Init 0 */   /* USER CODE END FMC_Init 0 */  ...

Aarra.1 by Senior
  • 1014 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F103C8, How to stop PWM signal?

Hi ST Community.I need your help. I am working on a PWM Proyect, Duty cicle must be change every period, and there is delta time where the PWM must be OFF.I am using a Timer, it fire an interrution and this interruption set a flag to 1 in order to r...

ERABALF by Associate III
  • 4353 Views
  • 5 replies
  • 0 kudos

i2c1 block with DMA is not working (STM32h743) - when the first transaction is sent from master board to slave board - > the i2c1_event interrupt is triggered and it is stuck in an endless loop.

i've created 2 threads - i2c_tx_dma and i2c_rx_dma which use the HAL_I2C_Master_Transmit_DMA and HAL_I2C_Slave_Receive_DMA.I am working with 2 boards of the STM32h74 family:first board-> configured RX DMA on i2c1 block as a slave and activate HAL_I2C...

0693W00000Hno6oQAB.png 0693W00000Hno7rQAB.png 0693W00000Hno81QAB.png 0693W00000Hno8LQAR.png
VKats.1 by Associate II
  • 3170 Views
  • 7 replies
  • 0 kudos

QSPI bank2 <-> s/f memory is possible?

Hello,I have question about QSPI on stm32F446.I want to connect serial flash with QSPI.there are 2 banks on QSPI.When I try to find some example on QSPI, they were all used QSPI bank1 connected to s/f memory. But when I check pin connections on QSPI ...

Tiel by Associate II
  • 1282 Views
  • 3 replies
  • 0 kudos

Interfacing Stm32 with NXP controller over SPI.

I want to interface Stm32 MCU with a NXP MCU over SPI protocol.Does anyone have done that before?? If yes can you please tell me how it can be done? I have already used St and nxp mcus separately and now my application requires both of them together....

MGogr.1 by Senior
  • 3505 Views
  • 6 replies
  • 0 kudos

Resolved! Can the contents of RTC backup register become corrupted in case of VDD power reset while write operation is ongoing (VBAT is present)?

Hello ST Community,I am using RTC backup register of STM32F746ZG for saving some accumulating data.So i'm afraid of situation when i start write operation and in the same time the VDD power is disabled.Couldn't find any information about this, so i a...

Satty by Associate III
  • 1203 Views
  • 2 replies
  • 0 kudos