STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 UART shows inconsistent outputs

From what I understand, the UART gets a char/byte one by one. I am trying to test this by adding '-' between each character of the string I send to the UART. However, the outputted values are very inconsistent when more than 1 character is sent to th...

JTurn.2 by Senior
  • 5963 Views
  • 16 replies
  • 0 kudos

I am using STM32F030C6T6 I am unable to configure usart1 in the code. None of the registers get configured for usart1 below is the code Please Help. I am using Standard Peripheral Libraries.

void RCC_Configuration(void){   RCC_DeInit();  //RCC_AdjustHSICalibrationValue(0x00);  RCC_HSICmd(ENABLE);  while(RCC_GetFlagStatus(RCC_FLAG_HSIRDY) == RESET)    {;}  //PLL out = (8M/2)*12 = 48 MHz  RCC_PLLConfig(RCC_PLLSource_HSI_Div2,RCC_PLLMul_12)...

lernd by Associate II
  • 3662 Views
  • 5 replies
  • 0 kudos

CAN Bus strange signal (solved)

edit: the problem was due to a CAN-master switching baudrates on the fly.the wrong (slower) timing was detected by the CAN controller causing the interruption of the ongoing transmission.Hello Community !I am implementing CAN communication with an in...

0693W00000HpeihQAB.png

STM32:496 ADC1/2 dual mode, ADC3 independent?

I am using STM32L496 with ADC1/ADC2 in dual regular simultaneous mode with DMA and seeking to have ADC3 independent sinple single conversion. Code works either with ADC1/ADC2 or ADC3 but not with both. Can ADC3 run independent if ADC1/ADC2 are dual?

BSmit.2 by Associate
  • 906 Views
  • 1 replies
  • 0 kudos

How get timer state?

Hi,I´m reading the doc of my kits, stm32f767zi and stm32f429zi, but if anyone could help I´ll appreciate. I need start and stop a timer named htim3, as follow:if (HAL_OK!=HAL_TIM_Base_Start_IT(&htim3)) Error_Handler();But, if I execute the code twice...

Resolved! ADC Channel PreSelection

Hello what does this function do?( LL_ADC_SetChannelPreSelection(ADCx, Channel);),I couldn't find a detailed explanation.

Resolved! Unable to wake from Stop2 power mode with user button

I put my L4R5ZI chip into Stop2 mode but it doesn't seem to want to wake up from the user button, unfortunately. According to the datasheet, the wakeup sources include:Reset pin, all I/OsBOR, PVD, PVMRTC, IWDGCOMPx (x=1..2)I2C3(7)LPUART1(6)LPTIM1I h...

JayDev by Senior II
  • 1300 Views
  • 2 replies
  • 0 kudos

Resolved! Emulating a matrix keypad with a stm32 microcontroller

Good morning Stm32 community,I am designing a ​matrix keypad emulator to control a musical keyboard. I need a 16x16 keypad for the music keys and a 8x8 keypad for the control buttons. The idea is to swap the existing keypads connected to the existing...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.