Resolved! MTBF/FIT data of STM32L451RET6
Hi ST team,We are doing reliability calculations for our product so, we need data for STM32L451RET6.Can you please share this data?Thanks,Hitesh
Ask questions, find answers, and share insights on STM32 products and their technical features.
Hi ST team,We are doing reliability calculations for our product so, we need data for STM32L451RET6.Can you please share this data?Thanks,Hitesh
I bought 960 MCU very expensive.but many barcode and number has been deleted.I just wonder that this mcu is genuine or not
Couldn't use ITM for printf like debugging in STM32L432KC Nucleo 32 board
Hello and Happy New Year 2022,I'm using STM32L072, I set SPI1 to be in "Transmit Only Master" mode, and DMA1 as SPI1_TX (DMA1 Channel 3)I use CubeMX to Auto generate my codeThe relevant SPI1+DMA1 line is: HAL_SPI_Transmit_DMA(&hspi1, (uint8_t *)aBuff...
I have 2 types totally 4 boards (each type 2) of F103C6T6, I programmed them by ST-Link mini through CubeIDE, any of them could be only programmed once, the next time it would be prompted device could be found in CubeIDE. I mean is there any mechanis...
STM32F103STM32CUBEMX V4.25.1The slave device on my side is a fake PP output. It needs a pull-up resistor. I know this is not in accordance with the SPI agreement, but there is no way. When I run the HAL_SPI_Transmit() function, an incorrect pull-up s...
How to calculate audio signal from ADC in DMA using FFT to display on LED 10x10. I have STM32F411 DISCOVERY and connected left and right (2 channels) audio from smartphone. I found this guy https://www.youtube.com/watch?v=3WF4CGKoMas but his code opa...
Hello,During my exploration of the F401RE board, I tried to make the uart_printf example work correctly.Capturing the output of the main MCU via CN3-RX pin to a PicoScope 5440, an CH340 and on board F103 USB interface MCU all lead to the same conclus...
Has anyone transcoded the SHT30 Sensor for STM32L0 or any series? I didn't know how to adapt the I2C pins while exporting the libraries. For example how can I adapt these parts from arduino to stm32? link with library: https://github.com/Risele/SHT3x...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.