STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Two OSPI usage in STM32U599

Hello, Is it possible to use two OSPI with below configuration.  I can make this configuration in cubeMx but whiel debugging ospi1 is not working after ospi2 initialize.   

Epamuk_1-1777024547409.png Epamuk_2-1777024564617.png Epamuk_3-1777024580076.png Epamuk_4-1777024592601.png
Epamuk by Associate III
  • 226 Views
  • 3 replies
  • 1 kudos

Resolved! STM32N6 - booting off Quad spi (OTP) settings

Goal boot from a Quad SPI flashI shouldn't need to change any OTP settings.  Any sNor flash chip connected to XSPIM_P2 that can operated in single spi mode can be booted off from? From my understanding if we want to make a dev board and use a differe...

Screenshot from 2026-02-11 10-35-55.png Screenshot from 2026-02-11 08-57-46.png Screenshot from 2026-02-11 08-55-19.png Screenshot from 2026-02-11 10-17-46.png

STM32F105 DFU Bootloader Grief

Hi all.I'm new to STM, but have been designing and making embedded MCU products for over ten years.I was drawn to the STM32F105 series because of the USB DFU, to allow for field updates for prospective customers to update a product we're developing. ...

Tad_E by Associate II
  • 2407 Views
  • 6 replies
  • 0 kudos

Resolved! In Shutdown, how is RTC powered?

While I was experimenting with the 'L476 Disco, the RM wording goes across multiple families, so it may be relevant to most/all of them. In particular, for Shutdown mode (which is supposedly the lowest-VDD-consumption mode), the RM says: What does "...

Clipboard01.png

Resolved! Microcontroller with some kind of audio I/O capability ?

Split from WiFi or WiFi+BT modules architecture and parts recommendations as that's really a separate question!Thank you @Andrew Neil I didn’t explain myself very clearly. The part I’m mainly interested in is the audio side — specifically, a microcon...

Ricko by Senior III
  • 503 Views
  • 7 replies
  • 9 kudos

Resolved! STM32G071GBU6 top marking

(I tried to submit a ticket but the system seems broken, giving an obscure error about an incorrect zip code).I need to confirm which version of STM32 is placed on a board. There are two versions, GP and PD. The datasheet does not really specify how ...

pmillett_1-1776873894947.png STM32.jpg
pmillett by Associate
  • 173 Views
  • 2 replies
  • 0 kudos

STM32H753 Current Comsumption

Hello, in the STM32H753xI datasheet, Table 11, "Total current into sum of all VDD power lines (620mA)," is the voltage condition VDD = 3.3V? I would also like to know the current at VDD = 1.8V.

Koichi-H by Associate
  • 267 Views
  • 4 replies
  • 6 kudos