2025-07-27 6:09 PM
Whether the two buses can be used at the same time? Winbond's SDRAM is used to find a high probability of reading and writing errors in SDRAM data。 but there is no problem with using ISSI. If you don't read or write to the external SRAM, it's fine。
2025-07-27 6:18 PM
Yes, SRAM and SDRAM can be used at the same time. Try slowing the SDRAM clock rate down by a factor of 10, could be a layout or noise issue.