STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hi. I boot with stm32L010C6Tx. I am in standby mode. While waiting in standby mode, it shows between 3.1 micro amps and 50 micro amps 50 microamps is too high, I can't use it like this. . I turned off all peripherals. What else should I turn off? Why coul

void SystemClock_Config(void);static void MX_GPIO_Init(void);static void MX_LPUART1_UART_Init(void);static void MX_I2C1_Init(void);static void MX_ADC_Init(void);static void MX_RTC_Init(void);if (__HAL_PWR_GET_FLAG(PWR_FLAG_SB) != RESET) { __HAL_PWR_...

ZKURT.1 by Senior
  • 1489 Views
  • 2 replies
  • 0 kudos

Trigger SPI Read using Timer Update Event

Hello,I am trying to trigger each DMA read of my SPI to happen on update event Trigger output of my Timer but I don't think I have it setup correctly.I've seen this done using the internal ADC, where you can set the external conversion trigger source...

kcire L. by Associate III
  • 3565 Views
  • 3 replies
  • 0 kudos

Max voltage on pins when unpowered?

Hello,I notice in the STM32G030x6/x8 datasheet, Table 18 that the max input voltage on FT_xx and any other pin are VDD + 4V and 4V respectively. Does this mean those pins can be safely driven with 3.3V when the MCU is unpowered?Thanks,Nicholas

NLuon.3 by Associate
  • 1285 Views
  • 1 replies
  • 0 kudos

Resolved! RTC Reference Clock (50Hz) worsens the LSE accuracy

As indicated by an4759, I am trying to use the 50Hz mains reference to improve the RTC accuracy of an STM32F413ZH.However, the results I get are much worse than without using the reference:LSE only: 0.6s/dayLSE+50Hz: 7.5s/day (test duration 4 days)Ac...

0693W00000JPqz8QAD.png 0693W00000JPr5FQAT.jpg 0693W00000JPr8JQAT.jpg 0693W00000JPr8sQAD.jpg

Incomplete HAL_DMA_Abort_IT() in STM32F7xx_HAL v1.16

Hello,During a UART transfer I used the HAL_DMA_Abort_IT() function. The transfer stopped but the DMA handle stays locked and in the HAL_DMA_STATE_ABORT. When in this state the only thing to do is reinitialize the peripheral.Anyone have some feed bac...

ibobbymk by Associate
  • 731 Views
  • 0 replies
  • 0 kudos

ADC on ST Nucleo H743ZI board with DMA on Zephyr platform.

Hai, I am working with ST Nucleo H743ZI board for analog-to-digital conversion without CPU intervention between samples, by using DMA in Zephyr platform. Is there any ready-made example for the above, that I can refer?Thank you. Sachin

SJ.7 by Associate
  • 788 Views
  • 0 replies
  • 0 kudos

I have question on STM32F777 RTC and super cap

I wanted to use RTC Circuit for Supercap.I have designed circuit (Check Attached snapshot).but i dont get back up time? can anyone explain do we need to do any provision in controller.It seems that capacitor is discharging very fast

0693W00000JPlkbQAD.jpg
Chiku by Associate II
  • 1987 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.