Skip to main content
FTrom
Associate III
September 6, 2021
Question

Nuclel STM32F303K8 TIM2 as Encoder

  • September 6, 2021
  • 4 replies
  • 986 views

I'm working to read 2 identical encoders from 2 identical motor drivers.

I use TIM2 and TIM3 to read the encoders.

The encoder at TIM3 works properly, but the encoders at TIM2, I could see in debug mode the IRQ but the register CNT is zero. But every time that I restart the debug mode, I could read from CNT 1 and keep it.

Of course, I check the hardware (exchanging the cable and the motor drivers) but without any result. Plus from the software of the motor driver I can see the encoder to updated.

---------------------------------------- --------------------------------------------------------
main.c
---------------------------------------- --------------------------------------------------------
TIM_HandleTypeDef htim2;
TIM_HandleTypeDef htim3;
 
 MX_TIM2_Init();
 MX_TIM3_Init();
 
 HAL_TIM_Encoder_Start_IT(&htim2, TIM_CHANNEL_ALL);
 HAL_TIM_Encoder_Start_IT(&htim3, TIM_CHANNEL_ALL);
 
 while (1)
 {
 /* USER CODE END WHILE */
 
 /* USER CODE BEGIN 3 */
 }
 
----------------------------
 
static void MX_TIM2_Init(void)
{
 
 /* USER CODE BEGIN TIM2_Init 0 */
 
 /* USER CODE END TIM2_Init 0 */
 
 TIM_Encoder_InitTypeDef sConfig = {0};
 TIM_MasterConfigTypeDef sMasterConfig = {0};
 
 /* USER CODE BEGIN TIM2_Init 1 */
 
 /* USER CODE END TIM2_Init 1 */
 htim2.Instance = TIM2;
 htim2.Init.Prescaler = 0;
 htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim2.Init.Period = 65535;
 htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
 sConfig.EncoderMode = TIM_ENCODERMODE_TI12;
 sConfig.IC1Polarity = TIM_ICPOLARITY_RISING;
 sConfig.IC1Selection = TIM_ICSELECTION_DIRECTTI;
 sConfig.IC1Prescaler = TIM_ICPSC_DIV1;
 sConfig.IC1Filter = 0;
 sConfig.IC2Polarity = TIM_ICPOLARITY_RISING;
 sConfig.IC2Selection = TIM_ICSELECTION_DIRECTTI;
 sConfig.IC2Prescaler = TIM_ICPSC_DIV1;
 sConfig.IC2Filter = 0;
 if (HAL_TIM_Encoder_Init(&htim2, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN TIM2_Init 2 */
 
 /* USER CODE END TIM2_Init 2 */
 
}
 
static void MX_TIM3_Init(void)
{
 
 /* USER CODE BEGIN TIM3_Init 0 */
 
 /* USER CODE END TIM3_Init 0 */
 
 TIM_Encoder_InitTypeDef sConfig = {0};
 TIM_MasterConfigTypeDef sMasterConfig = {0};
 
 /* USER CODE BEGIN TIM3_Init 1 */
 
 /* USER CODE END TIM3_Init 1 */
 htim3.Instance = TIM3;
 htim3.Init.Prescaler = 0;
 htim3.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim3.Init.Period = 65535;
 htim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim3.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
 sConfig.EncoderMode = TIM_ENCODERMODE_TI1;
 sConfig.IC1Polarity = TIM_ICPOLARITY_RISING;
 sConfig.IC1Selection = TIM_ICSELECTION_DIRECTTI;
 sConfig.IC1Prescaler = TIM_ICPSC_DIV1;
 sConfig.IC1Filter = 0;
 sConfig.IC2Polarity = TIM_ICPOLARITY_RISING;
 sConfig.IC2Selection = TIM_ICSELECTION_DIRECTTI;
 sConfig.IC2Prescaler = TIM_ICPSC_DIV1;
 sConfig.IC2Filter = 0;
 if (HAL_TIM_Encoder_Init(&htim3, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim3, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN TIM3_Init 2 */
 
 /* USER CODE END TIM3_Init 2 */
 
}
 
---------------------------------------- --------------------------------------------------------
stm32f3xx_it.c
---------------------------------------- --------------------------------------------------------
/* External variables
extern TIM_HandleTypeDef htim2;
extern TIM_HandleTypeDef htim3;
/* USER CODE BEGIN EV */
extern int32_t enc_value2;
extern int32_t enc_value1;
 
void TIM2_IRQHandler(void)
{
 /* USER CODE BEGIN TIM2_IRQn 0 */
 
 /* USER CODE END TIM2_IRQn 0 */
 HAL_TIM_IRQHandler(&htim2);
 /* USER CODE BEGIN TIM2_IRQn 1 */
 enc_value1=TIM2->CNT;
 /* USER CODE END TIM2_IRQn 1 */
}
 
/**
 * @brief This function handles TIM3 global interrupt.
 */
void TIM3_IRQHandler(void)
{
 /* USER CODE BEGIN TIM3_IRQn 0 */
 
 /* USER CODE END TIM3_IRQn 0 */
 HAL_TIM_IRQHandler(&htim3);
 /* USER CODE BEGIN TIM3_IRQn 1 */
 enc_value2=TIM3->CNT;
 /* USER CODE END TIM3_IRQn 1 */
}
 

This topic has been closed for replies.

4 replies

waclawek.jan
Super User
September 6, 2021

Which pins?

Read out and check/compare/post content of TIM and relevant GPIO registers.

JW

TDK
September 6, 2021

> sConfig.EncoderMode = TIM_ENCODERMODE_TI1;

> ...

> sConfig.EncoderMode = TIM_ENCODERMODE_TI12;

If the encoders are identical, presumably the settings should be as well. Is this difference intentional?

"If you feel a post has answered your question, please click ""Accept as Solution""."
FTrom
FTromAuthor
Associate III
September 7, 2021

Hi, I have found my error. I had to remove the bridge SB15 of Nucleo

waclawek.jan
Super User
September 7, 2021

Thanks for coming back with the result.

Please Select your post as Best so that the thread is marked as solved.

JW