cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L011K4 internal data EEPROM write and read using Low Level (LL) driver

Swapnil1
Associate II

Hello,

I could't found example with Low Level driver to read-write from data EEPROM (FLASH).

I wrote some simple functions to read-write from data EEPROM.

If anyone have even simple solution, i would sincerely appreciate it.

Thanks!

Regards,

Swapnil

/**************************************************************** Data Read-Write from data EEPROM (FLASH) start *******************************************************************************/

#define EEPROM_BASE_ADDR    0x08080000  // Starting Address

#define EEPROM_BYTE_SIZE    0x01FF    // End address (512 Bytes)

uint8_t data_to_write[] = "LL Hello to EEPROM LL";     // write data buffer

uint8_t data_to_read[100];               // read data buffer

/* Write to EEPROM: */

void EEPROM_WRITE(uint16_t BiasAddress, uint8_t *Data, uint16_t len) 

{

 uint16_t i;                                   // counter i

 UnlockEeprom();                                 // Unlock the EEPROM

 FLASH->PECR = FLASH->PECR & ~(FLASH_PECR_ERASE | FLASH_PECR_DATA); // Reset the ERASE and DATA bits in the FLASH_PECR register to disable any residual erase 

 for(i=0;i<len;i++)

 {

  FLASHEx_DATAEEPROM_Program(EEPROM_BASE_ADDR+BiasAddress+i, *Data);      // call fun to write data to EEPROM

  Data++;                                    // Data increment

 }

 LockEeprom();                                  // Lock the EEPROM

}

FLASHEx_DATAEEPROM_Program(uint32_t Address, uint32_t Data)

{

   *(__IO uint8_t *)Address = (uint8_t) Data; // Program byte (8-bit) at a specified address.

    __WFI();                     //Enter in wait for interrupt. The EOP check is done in the Flash ISR

}

/* Lock the EEPROM: */

void LockEeprom(void)

{

 while ((FLASH->SR & FLASH_SR_BSY) != 0) // Wait for FLASH to be free 

 {

  // insert timeout test 

 }

  FLASH->PECR = FLASH->PECR & ~(FLASH_PECR_ERRIE | FLASH_PECR_EOPIE); // disable flash interrupts 

  FLASH->PECR = FLASH->PECR | FLASH_PECR_PELOCK;    // Lock memory with PELOCK */

}

/* Unlock the EEPROM: */

void UnlockEeprom(void)

{

 while ((FLASH->SR & FLASH_SR_BSY) != 0) // Wait for FLASH to be free 

 {

// insert timeout test 

 }

 if ((FLASH->PECR & FLASH_PECR_PELOCK) != 0) // If PELOCK is locked 

 {

 FLASH->PEKEYR = 0x89ABCDEF; // Perform unlock sequence this sequence is used to unlock the data EEPROM and the FLASH_PECR register

 FLASH->PEKEYR = 0x02030405; // Perform unlock sequence this sequence is used to unlock the data EEPROM and the FLASH_PECR register

 }

 FLASH->PECR = FLASH->PECR | (FLASH_PECR_ERRIE | FLASH_PECR_EOPIE); // enable flash interrupts 

}

/* Read from the EEPROM: */

void EEPROM_READ(uint16_t BiasAddress,uint8_t *Buffer,uint16_t Len)

{

uint8_t *wAddr;                             // pointer to written address data

wAddr=(uint8_t *)(EEPROM_BASE_ADDR+BiasAddress);            // store data in var wAddr

while(Len--)

{

*Buffer++=*wAddr++;                       // store data from var wAddr to read data buffer        

}

}

int main(void)

{

 EEPROM_WRITE(0x08080000,data_to_write, strlen((char *)data_to_write)); // Write to EEPROM

 EEPROM_READ(0x08080000,data_to_read,50);                    // Read from EEPROM

 while (1)

 {

 }

}

/**************************************************************** Data Read-Write from data EEPROM (FLASH) end *******************************************************************************/

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0