User Activity

Im struggling with USB Device RNDIS example . Works fine on Windows PC, but no network interface appears on Linux, it listed in lsusb output.I cant find any topics related to that issue
I have a packet communication via 2 devices over SPIAt the end of some packets I receive some extra clocks via SPI, therefore it corrupts the next packet. Situation can be discovered by BUSY flag set. Datasheet says it is cleared by hardware. Is the...
I've been struggling with this for a while. Is there a good tutorial on how to setup and configure debug printf output? STM32H743 all parameters on pictures attached. No output on printf function + Trace: Data Overflow text in status bar. And on top ...
Got a problem with ethernet on my custom board with STM32H743BIT and DP83848 PHYeverything 'seems' to work, but I see no outgoing traffic from my board on wireshark.Rx working though, screenshots attached.I read an articlehttps://community.st.com/s/a...
Is there STM32G4 USBD CMSIS Driver? Because latest (1.5.0) package for G4 doesnt include it. There is an example for CDC, but nothing for CMSIS and RTOS. Seems kinda weird.
Kudos given to