User Activity

Good afternoon, I have written two versions of the time output test programs to the console for STM32MP157D. Both programs work no more than 2 hours, then the system restarts. What did I do wrong?Sincerely, Alexander. ////////////////////////////////...
Good afternoon.I tried to create a demo project (STM32MP157C-DK2\Demonstrations\Al_Character_Recognition) for the STM32MP157D_DK1 board. When assembling, I had a problem.(Gluk_test_1) How to include the library in the project correctly? Sincerely, Al...
Good afternoon, I wrote a program for controlling the railway scoreboard in Python 3 for the STM32MP157A-DK1 board. I have a problem. It is described by the link https://bugs.launchpad.net/ubuntu /+source/gnome-control-center/+bug/1264368Troubleshoot...
I have a problem. My application should use port 8888. I wrote an application in Python 3.5 that uses the address and port 8888 that I need. But Linux issues a diagnosis that port 8888 is already occupied by another task. How to release port 8888.? T...