STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 Compilation issue with gnc gcc

Hello All,I am working on the STM32 project and using the makfile to compile and generate respective hex and bin files.I have configured all the setups using adding path in windows10 os environment variables for makefile and gnu gcc compiler.It compi...

0693W00000Lx0FmQAJ.png
SSing.10 by Associate II
  • 2982 Views
  • 5 replies
  • 0 kudos

How to receive a variable length data using USART and DMA?

Hello!I'm trying to receive a varible length data in USART2 and then send by USART1, but I receive the data and then a lot of spaces or newline characters. Also, i tried to use callbacks but the output characters are wrong. I even have read about a r...

SGonz.2 by Associate II
  • 2131 Views
  • 4 replies
  • 0 kudos

Where are the .ioc files for STSW-STLKT01 sample programs?

According to the data brief STSW-STLKT01 Embedded software samples for SensorTile (DB2962) the sample projects are "Built on STM32Cube software technology, it includes all the low level drivers to manage the on-board devices and system-level interfac...

HCohe.1 by Associate III
  • 1025 Views
  • 1 replies
  • 1 kudos

Resolved! Lock Process or Priority (what is strongest)

Let's assume we have a software that uses FDCAN Classic and I2C with multiple slaves. FDCAN Priority = 1I2C Priority = 2During the transmission / Receiving process, the I2C is locked : __HAL_LOCK(hi2c);If an FDCAN interruption arrives during the I2C ...

MAmem.1 by Associate III
  • 1214 Views
  • 2 replies
  • 0 kudos

[H730] FDCAN Transmitting messages leads bus to off state

Bus speed - 100kbit/s in CAN 2.0 modeFDCAN clk - 48MhzPrescaler - 24 (bit length 20tq)TQ1 - 15 (sample point 80%)TQ2 - 4SJW - 4Receiving CAN messages without any problems, bus seems to be ok, even if FDCAN in normal mode(error counters are 0). But if...

AAlex.20 by Associate II
  • 2073 Views
  • 3 replies
  • 0 kudos

Read and write SDRAM using Dual Core STM32H7

Hello, I have been working with STM32H7 microcontrollers for a while now but have always used the single core. Now I want to use the Dual core to read and write data in the external SDRAM. I have looked through all materials available online but c...

Aarra.1 by Senior
  • 1708 Views
  • 2 replies
  • 0 kudos

Resolved! STM32L451RC are there Problems known for the BSDL File? I tried to do a Boundary Scan but it is not possible to set the Pins I want. I try to write 334 Bit but If I change the state ob a Pin from outside, I see that this Pin appears 120 Cells before.

That is what I send for exsample:SIR 9 TDI (0);SDR 334 TDI (49000000001249240a49249248000000000001249200000000000249249249008000000001249200) SMASK (3fffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffff) TDO (0) MASK (0...

MDebu.1 by Associate II
  • 3057 Views
  • 6 replies
  • 1 kudos

Dear Community members, I am writing code from scratch to glow LED present in PC13 of STM32F103C(Blue pill) but the LED is not getting turned ON. Kindly help me with this. I am attaching the code below.

Code://LED//Pin:C//Pin Num:13#define PERIPH_BASE (0x40000000UL)#define APB2_OFFSET (0x00010000UL)#define APB2BASEADD (PERIPH_BASE + APB2_OFFSET)#define GPIOC_OFFSET (0x1000UL)#define GPIOC_BASE (APB2BASEADD+GPIOC_OFFSET)#define AHB_OFFSET (0x18000UL)...

SVemp.2 by Associate II
  • 3303 Views
  • 6 replies
  • 0 kudos