STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Unable to connect to F103 MCU

Hi, I forgot to add the  pins in my STM cube project and flashed my MCU. Now I am not able to connect to my MCU. I am working with the STMF103RCT6 MCU. I tried giving 3.3V to the boot pin and connect a UART to serial converter  to my board. But it st...

Screenshot from 2025-08-29 12-07-26.png

HRTimer "Roll Over" synchronization

The way the ref manual states this makes it sound like, if, before you start a counter, you "manually" set the counter to a value higher than the period value, it will NOT start counting / reset back to zero once the timer is actually enabled. Howeve...

Jbin0101_0-1756398558523.png
Jbin0101 by Associate III
  • 527 Views
  • 1 replies
  • 0 kudos

Gpio status during bootmode

Hi,  I am working in STM32G491, currently working on MCU firmware upgrade part. I have a doubt regarding the output pins. Currently we have SET 2 GPIOs to high. That is power enable for another device say A. From another external device B, it is cont...

Resolved! SPI on STM32C011J4M6

Hello. I'm trying to configure the STM32C011J4M6 to output SPI in Transmit Only Master mode. However, as soon as I turn on SPI in STM32CubeIDE and program it, the uC stops behaving properly. I can't transmit any data and the clock pin stays high with...

I3C Master RX length > Slave TX length

I am using two  NUCLEO-U385RG-Q boards for I3C communication—one as the Controller (Master) and the other as the Target (Slave). When the Controller’s RX length exceeds the Target’s TX length, after the first call to HAL_I3C_Ctrl_Receive_IT the Contr...

bell_huang_0-1756106814010.png bell_huang_1-1756106824360.png bell_huang_2-1756106862218.png bell_huang_3-1756106871530.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.