STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Six SPI continuously monitoring

Hello, I am working on STM32H7 series controller, I have to continuously reading the data of dac through spi and vtg ,and send over an GUI application so every 50 microsecond I have read the values of 6 spi , so I have do the calculation in stm32 or ...

MDeva.1 by Associate II
  • 1849 Views
  • 4 replies
  • 0 kudos

Is the STM32F43x underlying chinas import/export regulations?

Is the STM32F43x under any import/export regulations, if you want to export a product with F43x to china? Because for example china has theyre import and export list for crypto devices. Or in regard of Wassenaar Arrangement? Even tho our product does...

CButz.1 by Associate III
  • 2105 Views
  • 3 replies
  • 0 kudos

How do I create an Interrupt for UART_FLAG_TXE?

I have a STM32L081KZT and I am using the LPUART.I want to create my own Interrupt (handler) based on UART_FLAG_TXE. So basically a function that gets called whenever the UART_FLAG_TXE bit is set.In the GCC compiler manual I have found this:void f () ...

HRaup.1 by Associate II
  • 2068 Views
  • 3 replies
  • 0 kudos

What would be a modern equivalent to an STM32F103, preferably in a 48 pin package, and which wouldn't require too many alterations to existing code and PCB?

I've spent the last 2 years developing a product using an STM32F103, but I've recently discovered that the ones I've been supplied with are fakes, which have a tendancy to blow up :( It seems as if no genuine F103s are available now, so either I have...

SCook.1 by Associate III
  • 5055 Views
  • 8 replies
  • 1 kudos

STM32F4 TXE flag not activating

We have a very simple, blocking, UART transmit routine, which writes a byte and waits for TXE to become active. Every so often, and I mean something like 1 in 100,000 or more calls, it gets stuck at line 3 of the code pasted in below; TXE never becom...

STM32 lower power consumption

Hi everyone, I need the lowest possible current consumption for my project. I need to power my MCU with external supply. Currently I have a Nucleo F401RE, which is not so good for low power applications it seems. It's connected to a X-NUCLEO-NFC04A1 ...