Visitor II
December 15, 2021
Solved
FDCAN - 2 Nucleo G0B1RE Board - What i am doing wrong ?
- December 15, 2021
- 1 reply
- 941 views
Hello,
I am currently working with 2 Nucleo-G0B1RE board. I adapted the "FDCAN_Com_IT_2_BOARDS" from the G0C1RE-EV example.
Clocks are the same, so i think the fdcan is properly setup.
I changed the RX/TX pin from PD12/PD13 to PA11/PA12, and connected the 2 board together, without using FDCAN transceiver, just using RX/TX pin.
When using FDCAN_MODE_EXTERNAL_LOOPBACK mode, my signal looks fine, but in normal mode, i always get a bit error (first transmission).
What i am doing wrong ?
Thanks for your help