STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

g051 serial problem

HiI have made a board using the g051k6 chip. I have not been able to receive data from another board sending data at 115200 bd. I connected another serial port to the input pin , and all data is received without errors. A uart problem is mentioned...

kevint1 by Associate
  • 1405 Views
  • 3 replies
  • 0 kudos

stm32f303rc: SRAM parity error bit NOT SET, but NMI is taken

SRAM parity check is enabled. In fact, breakpoint in NMI is reached.But SYSCFG_CFGR2.SRAM_PEF bit is NOT set. See .png.Disassembly (at bottom) shows, that address of CFGR2 is loaded at R0 ("Registers" to the right) and its contents is loaded to R1. T...

USeid.1 by Associate
  • 1674 Views
  • 2 replies
  • 0 kudos

STM32G0 ADC AWD2/AWD3 does not work

Hello everyone,we have a STM32G070CBT6 microcontroller and we want to use the ADC in the following configuration:Channels: 1,2,3Continuous Measurement, automatically restart at channel 1 after measuring channel 3Transfer measured analog values via DM...

mabe_rs by Associate II
  • 2477 Views
  • 2 replies
  • 0 kudos

Resolved! Switch from OctoSPI1 to OctoSPI2

Hello,currently we are successfully using an external NOR flash connect via Hyperbus on OCTOSPI1, ClockPort 1 for some time (~1.5 year).We would like to switch to OCTOSPI2 because we want to use the other address area (0x70000000UL instead of 0x90000...

TNeub.1 by Associate III
  • 1683 Views
  • 3 replies
  • 0 kudos

STM32L 32.7680Khz Clock Problem

Hello, after several Years of using the 32L475RET6 with a 12pF 32.7680KHz Crystal and 8.2pF Capacitors we need to change the PCB to a 32L486QG. As to read in the Datasheet both have 5pF Pin Input Capacity. But the new Design (Chrystal about 1.5mm awa...

GJaeg.1 by Associate II
  • 3033 Views
  • 8 replies
  • 0 kudos

Where can I get the correct macro names for .stldr file?

I'm trying to create my own .stldr file. I follow this instructionhttps://youtu.be/XqCq0xtQmbIAnd when I replace the default linker script with "my own", the code doesn't compile...Where can I get the correct macro names?PS - my board is: STM32H750VB...

DK.7 by Senior
  • 925 Views
  • 0 replies
  • 0 kudos

How to debug "STEP Over (F6)" SCB_ENABLEDCACHE ()?

I trying to debug my simple "Blink" code by pressing "STEP Over (F6)" but it freeze every time at SCB_ENABLEDCACHE ();But, if i press restart and "F8" (resume) everything working well!  My stm is STM32H750VBT6.

DK.7 by Senior
  • 1450 Views
  • 2 replies
  • 0 kudos