cancel
Showing results for 
Search instead for 
Did you mean: 

Has anyone workding SDRAM on H743zi2 Nucleo? in particular uing SDRAM IS42S16160J

MEdgerton
Senior

Has anyone workding SDRAM on H753zi2 Nucleo?

To start I have a F767 with the IS42S16160J working. Writes and reads back fine. Proven by disconnecting a line and the test code finds it.

Move to H743zi2. No joy, it just reads almost radom back.

I changed the clock of the H743 to match the F767 and the sam settings, but still no joy.

I did find going to STM32CubeIDE 1.6.1 there is a new RCC setting for the LDO that set it to 3 and slowed the clock so I coulnt get 480MHz, but setting to 0 fixes it (documeted elsewhere but not by ST). Altough backed off to 100 or 200 for memory tests.

T

hen I found the chip revision defaulted to Y but the chip physically says V. Any ideas?!

So there seems to be a lot of incorrect "defaults" in the new version.

I started a project from scratch - no jpy on the H743.

I have used IS42S16160J and IS42S16160G (both very similar)

Does anyone have working code on th H743 for SDRAM andthe MCettings to compare. So far I am lost!!!!!

Most of the pins do pulse (not D0 but it doesnt on the F767 unless I write slowly) when doing bytewise but using a 16bit byte address.

It still makes no sense why the same setup on both does not work.

I have checked through the boards and so far no shorts missing connections etc and thats 2 days checking.

Thank you!!!!

All suggestions and code welcome!

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
MMajc.1
Associate

Hi, were you able to make it work?

SKacp.1
Senior II

Hi,

Please see my example project STM32H743BIT and SDRAM IS42S16800F-7TL

Best Regards,

Slawek