User Activity

I have written a program in the STM32CubeIDE V1.16, creating a .elf file for the STM32H723.I then followed the Phils Lab tutorial https://www.youtube.com/watch?v=VlCYI2U-qyM to program the Nucleo development board using USB using STM32CubeProgrammer ...
I have been using the same project with the AI cube IDE (V 1.13) and AI (V8.1). When I now try to build the project I get the following errors:I've updated the AI to the newest version, but the error seems still here. The error also seems to be a cor...
I've updated my code to CubeAI 8.1. The middleware is still deleted... but I can add it manually. However when I build the code I gett the error:Description Resource Path Location Typecannot find -l:NetworkRuntime730_CM7_GCC.a AI_FILES_GENERATOR C/C+...
I am currently using the STM32 to sample a waveform with an ADC, perform the FFT and transmit the data to a computer. 2 ADC's are used, and the buffer fills up every 1.26 ms. The result of 12 FFT bins is transmitted to the PC, which is around 1400 bi...
I am currently trying to run an ML model on the STM32H7A3. The model is uploaded correctly and successfully analysed.The first issue is that when generating the code, the middleware folder which contains ST>ai (which contains ai_platform) is deleted ...
Kudos from
Kudos given to