STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

2 bit RTC->DR problem for STM32F767 (corrected title)

I am using STM32F767, unfortunately I have a problem with the DR register area in the RTC. Exactly the problem is with the 10th and 17th bits of this register. Setting "1" means that I am not able to change these bits to "0". Only resetting the BDCR ...

RKosst by Associate II
  • 20073 Views
  • 14 replies
  • 0 kudos

Resolved! STM32G030K6T6 is not programming!

Hello,I'm working on a small scale project. In my earlier design, I've used the STM32F100x series. Now as the STM introduced a new set of controllers, the STM32G series ( which is less in cost and much higher efficiency than STM32F series), I've migr...

How to use printf() to output to UART

I have been using printf() to output to UART for many years on a STM32L052All these projects still compile and printf() to UART, no problem.I started a NEW project with CubeMX, but now printf() does NOT print to UART.I use the same int fputc(int ch, ...

gerhard by Associate II
  • 22424 Views
  • 12 replies
  • 0 kudos

MT29F128G08 NAND FLASH with NUCLEO-L496ZG basic driver help

I am not much of a software/firmware developer, but i need to get a basic Driver working for NAND flash device "MT29F128G08AJAAAWP-ITZ" working on a "NUCLEO-L496ZG".I have the device wired up to the eval board, and need to build a basic drive to writ...

RWarn.1 by Associate
  • 1958 Views
  • 3 replies
  • 1 kudos

What is the correct maximum FMC clock on a STM32F767 ?

Hi, I am currently working on a display driver board, with a STM32F767. And I would like to use the FMC with a SDRAM.My problem is that the MCU is clocked at 216MHz, the SDRAM max clock is 133MHz, on the F767 documentation, it is written that the max...

SylvainF by Associate
  • 2666 Views
  • 3 replies
  • 0 kudos

g051 serial problem

HiI have made a board using the g051k6 chip. I have not been able to receive data from another board sending data at 115200 bd. I connected another serial port to the input pin , and all data is received without errors. A uart problem is mentioned...

kevint1 by Associate
  • 1413 Views
  • 3 replies
  • 0 kudos