STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to debug "STEP Over (F6)" SCB_ENABLEDCACHE ()?

I trying to debug my simple "Blink" code by pressing "STEP Over (F6)" but it freeze every time at SCB_ENABLEDCACHE ();But, if i press restart and "F8" (resume) everything working well!  My stm is STM32H750VBT6.

DK.7 by Senior
  • 1449 Views
  • 2 replies
  • 0 kudos

How to fill ram with pattern in loading and before runtime?

Hello guys,I am using the stm32f446re discovery board, my aim is to measure the ram consumption of my application. The first approach is to use the static stack analyzer checking the memory details, the second approach is to fill the memory with a pa...

Mrahm.2 by Associate II
  • 3437 Views
  • 4 replies
  • 0 kudos

Option Bytes

hello,The option byte is configured with read and write protection, but I can program without erasing, why?FLASH_OBR = 0x03FFFFFAFLASH_WRPR = 0xFFFF0000

shan chen by Associate II
  • 1569 Views
  • 4 replies
  • 0 kudos

Resolved! Sometimes, WWDG was not working and CPU hang

My company uses the STM32G0071CB chip. but I faced some issue.whenever I need to reboot main board, I have to reset the STM32G0071CB as wells.so I used the WWDG for resetting the chip.But sometimes, chip was not reset and CPU hang.(once a 400 times o...

Andy.kim by Associate
  • 2040 Views
  • 3 replies
  • 0 kudos

UART DMA Rx STM32H745 with LL

Hello,I have tried implement UART Driver only with LL Library. I'm using Nucleo-H745ZIQ. Reception through DMA is not happening. Data is not getting copied to the buffer. MPU Also Configured. I'm attaching the code. Hope DMA Configuration for Rx is o...

veera1 by Associate II
  • 3740 Views
  • 4 replies
  • 0 kudos

Connecting two nucleo boards using I2C.

Hello, I just started using the Nucleo board and currently I am trying to connect two Nucleo G071RB by using I2C, using one as a Master and another one as a Slave.I, however, am not able to even get a clock signal coming from the Master (measured usi...

MC.4 by Associate II
  • 2934 Views
  • 2 replies
  • 0 kudos