STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

When the external 5V power of the STM32H735g-dk board is supplied, intermittently, the initial reset does not work normally.

When the external 5V power of the STM32H735g-dk board is supplied, intermittently, the initial reset does not work normally.​STM32H735g-dk​CubeIDE​Downloading the latest version of CubeIDE and CubeProgrammer does not solve the problem.​​If the initia...

mSH.1 by Associate III
  • 866 Views
  • 0 replies
  • 0 kudos

STM32F446ZET6 - Struggling to get the CAN running

Hi,I'm struggling to get the CAN working on a project I'm working on with the STM32F446ZET6. With the project below (CastletRestart) i just get a flat line of 3.3V high on the TX line for CAN1, this is being tested in loop back mode, with the TUT_CAN...

CBrun.5 by Associate II
  • 675 Views
  • 0 replies
  • 0 kudos

Using OnePulse mode with Repetition Counter on STM32G4 HRTIM

I have an application which I prototyped on an STM32L476. It works fine, but I need to move up to an STM32G4 since I need extra processing power. I am driving the ADCs quite fast (5.35MHz) and need to use HRTIM to get the sampling times right (sampli...

DMcin.11 by Associate II
  • 4957 Views
  • 7 replies
  • 0 kudos

ADC Common-mode range

Hello, I am trying to understand the common-mode range in differential mode - according to the data-sheet, it looks like it is quite narrow:Could you please clarify?We wish to wok with 0 to 2.5 V signals.Thanks.

0693W00000QNGk5QAH.jpg
Sharon by Associate II
  • 4219 Views
  • 9 replies
  • 0 kudos

unique die and device identifier

Hi, STM32 has a unique device identifier and unique die identifier. is there any possibility to read the value of those ids and also to change their value? Thanks

TLit.1 by Associate
  • 1520 Views
  • 2 replies
  • 0 kudos

Resolved! how to use TIM3_ETR to remap TIM3_CHx

Hi all,I haven't worked with ETRs earlier. I am currently working with stm32G491, I want to use TIM3_CHx, as an input capture. due to design problems, I am not available to use those pins. but I can use the TIM3_ETR pin. so is it possible to remap to...

0693W00000QNT89QAH.jpg
Roshan by Associate III
  • 1936 Views
  • 1 replies
  • 0 kudos

How I can program STM32U5 via USART from Embedded Linux?

Hi,I've used stm32flash on my processor with embedded Linux to program STM32U5 via USART. When I enter a command ./stm32flash /dev/ttymxc0 (usart interface connected to the STM32U5). I got a message "Failed to init device".On the stm32flash site I fo...

ASavi.3 by Associate II
  • 2046 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.