User Activity

Hello all, I want to take ADC reading at regular intervals based on timer 1 (used OC mode). The timer must trigger the ADC to take a reading and the ADC in turn will trigger the DMA to transfer the ADC reading to memory. To check that the timer is ru...
Hi all,Installed the latest CubeIDE and re-built an existing project. Got several warnings. One of them was RWX. This could be solved by making changes to the ,ld file. Example - .ARM (READONLY)The next issues was -- > "_close is not implemented and ...
Hello all,First of all, thank you all for helping and educating me on various topics whenever I needed help. This post is on how to rename an output file based on a define in my code. I understand this can be done by bash command(s) post-build, but a...
and build analyzer is showing those memory regions. I did not have this problem before. The new project name is AC_2 which is changed from AC_1. Now under build analyzer I see AC_1.elf/AC_2/Debug -27th August -2022, 6:33:40 PM. When I expand the proj...
Kudos from