cancel
Showing results for 
Search instead for 
Did you mean: 

Question about power control on STM32L476 Nucleo-64

EAmbr.1
Associate

Really new to programming these boards, and part of my project is to turn on/off these DC fans . I don't want to add any hardware to incorporate a switch, and was wondering if there was a way to program one of the power pins to be enabled or disabled so that the fans turn on and off strictly through Keil when a certain event happens. Haven't been able to find much about it online, any help is greatly appreciated.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
MM..1
Chief III

Simple reply no.

Maybe when your DC fan current meet for example 60mA , you can control it with GPIO one or more...

TDK
Super User

Generally, DC fans require more current (and voltage) than a GPIO pin can provide. Depends on the fan.

If you feel a post has answered your question, please click "Accept as Solution".