STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32U5 Burst length vs FIFO size

Hi all, i am going through deeper configuration of GPDMA on STM32U5 and there are some things i do not understand.S/DBL_1 in TR1 register is able to vrite destination/source burst length in range 0-63 but FIFO size is 8 bytes for channels 0-11 and 32...

Eiffel by Senior
  • 887 Views
  • 3 replies
  • 0 kudos

Resolved! FDCAN tx & rx FIFO size

Is there a way to set the FDCAN TX and RX FIFO sizes for STM32H7R7 in CubeIDE?I snooped around and found a list of macros that are responsible for determining the FDCAN RAM size in the stm32h7rsxx_hal_fdcan.c. Do I just modify these values to set the...

Screenshot 2025-09-13 at 12.44.55 AM.png Screenshot 2025-09-13 at 12.36.12 AM.png
Kwame by Associate II
  • 1336 Views
  • 3 replies
  • 1 kudos

Resolved! STM32G491KCU3/6 Differences

I found https://community.st.com/t5/stm32-mcus-products/stm32g491kxu6-don-t-have-exposed-die-pad/m-p/625099#M231656 on differences between STM32G491KCU3 and KCU6. Is junction temperature range the only difference between these parts?

STM32 power consumption in reset

I would need to know how much power does an STM32G0 consume when kept in reset by pulling down the RST pin.Is it specified somewhere?I'm afraid it might be more than what the part uses running a well power optimized software, right?