Skip to main content
Associate
March 26, 2025
Solved

STM32F405RGT6 and CAN not working

  • March 26, 2025
  • 5 replies
  • 1077 views

I try to get the CAN working. But currently I'm not sure what I'm missing.

I use the STM32CubeIDE v1.18.0. The boards I use is own hardware with SN65HVD232.

The hardware seems to work well. on the picture you see the screenshot from my oscilloscope, CANTX, CANRX, CANL, CANH after calling:

HAL_CAN_AddTxMessage(&hcan1, &TxHeader, &TxData[0], &TxMailbox)

The complete code is here:

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2025 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include <stdlib.h>
#include <stdio.h>
#include <string.h>
#include <inttypes.h>
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
#define TX_BUF 			 48
#define RX_BUF 			 16

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
CAN_HandleTypeDef hcan1;

UART_HandleTypeDef huart2;

/* USER CODE BEGIN PV */
uint8_t u8TxBuf[TX_BUF];
uint8_t u8Message[RX_BUF];
uint8_t u8RxBuf[RX_BUF];
uint8_t u8Receive[RX_BUF];
uint8_t	u8MsgAvl = 0;
uint8_t	u8RxCnt = 0;


CAN_TxHeaderTypeDef TxHeader;
CAN_RxHeaderTypeDef RxHeader;

uint32_t TxMailbox = 0;

uint8_t TxData[8];
uint8_t RxData[8];

uint32_t msg_count = 0;

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART2_UART_Init(void);
static void MX_CAN1_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */
	HAL_StatusTypeDef HALstat;
 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_USART2_UART_Init();
 MX_CAN1_Init();
 /* USER CODE BEGIN 2 */
 CAN_FilterTypeDef canfilterconfig;

 canfilterconfig.FilterActivation = CAN_FILTER_ENABLE;
 canfilterconfig.FilterBank = 0; // anything between 0 to SlaveStartFilterBank
 canfilterconfig.FilterFIFOAssignment = CAN_RX_FIFO0;
 //canfilterconfig.FilterIdHigh = 0x103<<5;
 canfilterconfig.FilterIdHigh = 0x0000;
 canfilterconfig.FilterIdLow = 0x0000;
 //canfilterconfig.FilterMaskIdHigh = 0x1<<13;
 canfilterconfig.FilterMaskIdHigh = 0x5000;
 canfilterconfig.FilterMaskIdLow = 0x0;
 canfilterconfig.FilterMode = CAN_FILTERMODE_IDMASK;
 canfilterconfig.FilterScale = CAN_FILTERSCALE_32BIT;
 canfilterconfig.SlaveStartFilterBank = 13;
 HALstat = HAL_CAN_ConfigFilter(&hcan1, &canfilterconfig);

 HALstat = HAL_CAN_Start(&hcan1);

 HAL_CAN_ActivateNotification(&hcan1,CAN_IT_RX_FIFO0_MSG_PENDING);
 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {

	 HAL_GPIO_TogglePin(GPIOB,GPIO_PIN_0);
	 if(0 != u8MsgAvl) {
			u8MsgAvl = 0;
			/*clear the answer buffer*/
			memset(&u8TxBuf[0], 0, TX_BUF);
			/* auswerten, was in der Nachricht stand*/
			switch(u8Message[0]){
				case 'F':

					sprintf((char*) &u8TxBuf[0],"F ok\r");
					break;
				case 'R':

					sprintf((char*) &u8TxBuf[0],"R ok\r");
					break;
				case 'L':

					sprintf((char*) &u8TxBuf[0],"T ok\r");
					break;
				case 'S':

					sprintf((char*) &u8TxBuf[0],"S ok\r");
					break;
				case 'X':

					sprintf((char*) &u8TxBuf[0],"X ok\r");
					break;
				case 'P':
					sprintf((char*) &u8TxBuf[0],"P ok\r");
					break;
			}
			HAL_UART_Transmit_IT(&huart2, &u8TxBuf[0], strlen((char*)u8TxBuf));
			HAL_Delay(5);
	 }
	 HAL_Delay(1000);
	 TxHeader.DLC = 4;
	 TxHeader.ExtId = 0;
	 TxHeader.IDE = CAN_ID_STD;
	 TxHeader.RTR = CAN_RTR_DATA;
	 TxHeader.StdId = 0x104;
	 TxHeader.TransmitGlobalTime = DISABLE;

	 if (HAL_CAN_AddTxMessage(&hcan1, &TxHeader, &TxData[0], &TxMailbox) != HAL_OK)
	 {
		 Error_Handler();
	 }

 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage
 */
 __HAL_RCC_PWR_CLK_ENABLE();
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 RCC_OscInitStruct.PLL.PLLM = 8;
 RCC_OscInitStruct.PLL.PLLN = 168;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4;
 RCC_OscInitStruct.PLL.PLLQ = 4;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief CAN1 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_CAN1_Init(void)
{

 /* USER CODE BEGIN CAN1_Init 0 */

 /* USER CODE END CAN1_Init 0 */

 /* USER CODE BEGIN CAN1_Init 1 */

 /* USER CODE END CAN1_Init 1 */
 hcan1.Instance = CAN1;
 hcan1.Init.Prescaler = 42;
 hcan1.Init.Mode = CAN_MODE_NORMAL;
 hcan1.Init.SyncJumpWidth = CAN_SJW_1TQ;
 hcan1.Init.TimeSeg1 = CAN_BS1_1TQ;
 hcan1.Init.TimeSeg2 = CAN_BS2_1TQ;
 hcan1.Init.TimeTriggeredMode = DISABLE;
 hcan1.Init.AutoBusOff = DISABLE;
 hcan1.Init.AutoWakeUp = DISABLE;
 hcan1.Init.AutoRetransmission = DISABLE;
 hcan1.Init.ReceiveFifoLocked = DISABLE;
 hcan1.Init.TransmitFifoPriority = DISABLE;
 if (HAL_CAN_Init(&hcan1) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN CAN1_Init 2 */

 /* USER CODE END CAN1_Init 2 */

}

/**
 * @brief USART2 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_USART2_UART_Init(void)
{

 /* USER CODE BEGIN USART2_Init 0 */

 /* USER CODE END USART2_Init 0 */

 /* USER CODE BEGIN USART2_Init 1 */

 /* USER CODE END USART2_Init 1 */
 huart2.Instance = USART2;
 huart2.Init.BaudRate = 115200;
 huart2.Init.WordLength = UART_WORDLENGTH_8B;
 huart2.Init.StopBits = UART_STOPBITS_1;
 huart2.Init.Parity = UART_PARITY_NONE;
 huart2.Init.Mode = UART_MODE_TX_RX;
 huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart2.Init.OverSampling = UART_OVERSAMPLING_16;
 if (HAL_UART_Init(&huart2) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN USART2_Init 2 */

 /* USER CODE END USART2_Init 2 */

}

/**
 * @brief GPIO Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 /* USER CODE BEGIN MX_GPIO_Init_1 */

 /* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOH_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();
 __HAL_RCC_GPIOC_CLK_ENABLE();

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6|GPIO_PIN_7, GPIO_PIN_RESET);

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOB, GPIO_PIN_0, GPIO_PIN_RESET);

 /*Configure GPIO pins : PA4 PA5 */
 GPIO_InitStruct.Pin = GPIO_PIN_4|GPIO_PIN_5;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /*Configure GPIO pins : PA6 PA7 */
 GPIO_InitStruct.Pin = GPIO_PIN_6|GPIO_PIN_7;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /*Configure GPIO pin : PB0 */
 GPIO_InitStruct.Pin = GPIO_PIN_0;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 /*Configure GPIO pins : PC10 PC11 PC12 */
 GPIO_InitStruct.Pin = GPIO_PIN_10|GPIO_PIN_11|GPIO_PIN_12;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

 /* USER CODE BEGIN MX_GPIO_Init_2 */

 /* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */
/**
 * @brief UART Rx IRQ function.
 *
 * The UART is configured to call this function for each received
 * character. Here the characters will be collected until CR received.
 *
 *
 * @PAram huart UART handle
 * @retval None
 */
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
	u8Receive[u8RxCnt] = u8RxBuf[0];
	if(13 != u8Receive[u8RxCnt]) {
		HAL_UART_Receive_IT(&huart2, &u8RxBuf[0], 1);
		u8RxCnt = u8RxCnt + 1;
		if(u8RxCnt >= RX_BUF) {
			u8RxCnt = 0;
		}
	} else {
		memcpy(&u8Message[0],&u8Receive[0],u8RxCnt);
		u8Message[u8RxCnt] = 0;
		u8MsgAvl = 1;
		u8RxCnt = 0;
		HAL_UART_Receive_IT(&huart2, &u8RxBuf[0], 1);
	}
	return;
}


void HAL_CAN_RxFifo0MsgPendingCallback(CAN_HandleTypeDef *hcan)
{
 //DBG("HAL_CAN_RxFifo0MsgPendingCallback");
 if (HAL_CAN_GetRxMessage(hcan, CAN_RX_FIFO0, &RxHeader, RxData) == HAL_OK) {
 //DBG("Got message %lu - id = 0x%04lx len = 0x%lx, data=%02x%02x%02x%02x%02x%02x%02x%02x", msg_count + 1, RxHeader.StdId, RxHeader.DLC, RxData[0], RxData[1], RxData[2], RxData[3], RxData[4], RxData[5], RxData[6], RxData[7]);
 }
 msg_count++;
}

/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @PAram file: pointer to the source file name
 * @PAram line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

I tried a lot of suggestions from this forum and also other examples. 

On a WeAct Module with quartz also not more than this one pulse on the CANTX appear. Where is my fault, what am I not seeing here?

I would expect at least a frame until the ACK.

This topic has been closed for replies.
Best answer by mƎALLEm

Hello,

Thank you for the sharing.

I suggest this timing configuration for a system clock of 42Mhz with 125kb/s a CAN bitrate standard value:

mALLEm_0-1742998679858.png

The updated ioc file in attachement.

5 replies

mƎALLEm
ST Technical Moderator
March 26, 2025

Hello @digitalMaik and welcome to the ST community,

I have a question and one remark:

Question: did you connect another node on the CAN bus? if nothing connected on the bus. That's an expected behavior. You need to connect another CAN node to acknowledge the frame.

Remark: 

These are bad timing parameters and most probably the issue comes from these values:

 hcan1.Init.Prescaler = 42;
 hcan1.Init.TimeSeg1 = CAN_BS1_1TQ;
 hcan1.Init.TimeSeg2 = CAN_BS2_1TQ;

 You need to increase BS1 and BS2 as much a possible and decrease the prescaler as much as possible where the sample point is between 75 to 85% of the bit time.

Could you please share your ioc file?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Associate
March 26, 2025

Thank you,

it's the same behavior if another node is connected. The speed is not so important, it it better for us, if the speed is slow.

The ioc-file is attached.  

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
March 26, 2025

Hello,

Thank you for the sharing.

I suggest this timing configuration for a system clock of 42Mhz with 125kb/s a CAN bitrate standard value:

mALLEm_0-1742998679858.png

The updated ioc file in attachement.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Ozone
Principal
March 26, 2025

As mentioned, CAN requires at least a second node to acknowledge reception.
So, first check if you meet this condition.

Second, each CAN node has internal error counters (TEC and REC). In addition to bus signals (scope), you can monitor those.

And in case of the firmware, I would start with loopback mode, progress to an connection on digital level (CAN Tx and Rx of the nodes connected directly, if levels allow it), and add CAN transceivers only at the last step.

Associate
March 26, 2025

Thank you very much.

Now I found it in the RM. Next time I should read the documentation and not only use standard values.