Skip to main content
Associate III
July 31, 2024
Question

STM Virtual Com port win11 driver needed

  • July 31, 2024
  • 12 replies
  • 40205 views

hello, where can i download win11 STM virtual com port?  i install both VCP_V1.5.0_Setup_w7_x64_64bits and W8_x86_32bit all not working ! i din see

STM Virtual Com port at device manager! only STM STLink visual com port appear ... 

12 replies

StanJermAuthor
Associate III
July 31, 2024

i m implementing my own USB VCP on a USB port (STM32 USB Virtual COM Port (VCP) )

https://medium.com/@pasindusandima/stm32-usb-virtual-com-port-vcp-bc7cb1bd5f5

StanJermAuthor
Associate III
July 31, 2024

i m using H734 Nucleo...

AScha.3
Super User
July 31, 2024

Hi,

the VCP driver :

https://www.st.com/en/development-tools/stsw-stm32102.html

should not be needed, as win10 + 11  have driver in system included - so maybe your enumeration going wrong...

or try thr driver - if you want.

 

If you feel a post has answered your question, please click on " Best Answer ".
StanJermAuthor
Associate III
July 31, 2024

hello... anyone can help ???

 

Pavel A.
July 31, 2024

Look for CDC device example in the Cube example projects for STM32H7, adapt it for your board.

 

Andrei Chichak
Lead
July 31, 2024

You don't need a VCP driver for late windows 8 forward. It just shows up as a COM port.

If your device isn't showing up, I'd suggest that there is something incorrect with your program running on the H7. You do have a program running on the H7, don't you? You have to provide a program that implements the device side of the VCP, it's not built into the H7.

StanJermAuthor
Associate III
August 1, 2024

yes.. i hav a program but seems its not working,,,

Visitor II
March 27, 2025

 I am facing similar issue , STM Virtual Com port not appearing at device manager when I  plug usb cable . Were you able to resolve this?

Visitor II
March 18, 2026

Having similar issues with the EVL6482H-Discovery board, latest firmware flashed shows up as a HID compliant barcode reader under windows 11.

HID\VID_0483&PID_7004&REV_0110
HID\VID_0483&PID_7004
HID\VID_0483&UP:008C_U:0001
HID_DEVICE_UP:008C_U:0001

It identifies as a HID compliant device with 2 endpoints