STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32C0 not driving CAN bus

STM32C092CCT6 : TCAN1463-Q1: TXD Dominant but No CAN Output — Bit0 Errors, nFAULT OK, Normal Mode Confirmed Hello everyone,I am facing an issue where the CAN transceiver (TCAN1463-Q1) does not drive the CAN bus even though the STM32 FDCAN peripheral ...

STM32G070RBT6 with external pull-up resistor having weird voltage level

Post edited by a ST moderator: 1- Translate the text to English. 2- Update the title to be more concise. 3- Update the label.   我在使用STM32G070系列芯片时,外部电阻上拉到3.3V,接入STM32芯片后测量,发现GPIOA 15 和GPIO A8两个引脚是0.9V的电压,为什么? Translation: "When using the STM32G070 se...

AAApink by Associate
  • 141 Views
  • 1 replies
  • 2 kudos

Resolved! Flash READ & WRITE works even beyond specified size!

Dear ST We are currently proceeding with development using the STM32H743VGT6.As you can see in the datasheet, the STM32H743VGT6 has a built-in 1M flash.I confirmed that it operates normally even though the flash partition was divided as shown below f...

hongjo_0-1776836448661.png hongjo_2-1776836842264.png hongjo_4-1776836990960.png hongjo_3-1776836887657.png
hongjo by Associate II
  • 275 Views
  • 5 replies
  • 7 kudos

STM32G0B1CBT3N vs STM32G0B1CBT6N

Hello Peter ,  Need your expert reply  As we see , the confusion on N AND no N HAS MADE many of us wonder , if these can be used as  interchangeable parts . Since Data Sheet does not explain , much on them ,But a search explains a compact Solution in...

Tintin33 by Associate
  • 118 Views
  • 1 replies
  • 1 kudos

Resolved! Voltage information on PA0 for STM32N657X0H3Q

Hello Team, We are using STM32N657X0H3Q for one of our application, while looking for the voltage level information for pins, we did not get any information for PA0 pin for the controller, specifically i am referring the notes column in pin descripti...

Harsh_Bhavsar_0-1776749020632.png