STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

what is the address on register A16

Post edited by ST moderator to be inline with the community rules especially with the code sharing. In next time please use </> button to paste your code. Please read this post: How to insert source code #define FMC_BANK1_BASE ((uint32_t)0x60000000) ...

MNapi by Senior III
  • 335 Views
  • 0 replies
  • 0 kudos

STM32U375RGT6Q - UART function

Hi,Will PC0 PC1 LPUART functions in normal operation? I have to use this LPUART in normal operation of MCU, not in power saving mode.Is there any limitation on this like speed, baud rate etc. Regards,Anurag    

ADC Fluctuation

Hello,I have a ADC clock running at 96MHz prescaler divided by 10, 12bit, Sampling time 47.5 Cycles. I am just trying to sample this DC volgtages.  I have a battery that has around 20Volts, and I am stepping this voltage down using the voltage divide...

ytshin0877_4-1758084688725.png ytshin0877_0-1758083861526.png ytshin0877_3-1758084135450.png

Resolved! STM32H725VGH6 / Direct SMPS Supply / VLXSMPS Connection

Hi,We are using the STM32H725VGH6 MCU and are plannign to use the internal SMPS for VCORE.With regards to the connections required for the VLXSMPS pin, I would just like to confirm that a 220pF capacitor is required on this pin in the "Direct SMPS Su...

Figure3.png Table2.png Figure2.png
SammExa by Associate
  • 4982 Views
  • 5 replies
  • 2 kudos

STM32G030C8T6 readout protection doesn't work

I tried to set readout protection via ST-LINK CLI - it's enabled and disabled correctly, but after RDP=0 I can't erase/write chip - I've got an error on write operation. Tested on 2 boards and both boards have same behavior. e:\STM32 projects>"%PROGR...

NiTr0man by Associate III
  • 897 Views
  • 5 replies
  • 2 kudos