STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

What is the maximum main frequency of the STM32H7 devices, and if this frequency can be output by any of the devices pin?

What is the maximum main frequency of the STM32H7 devices, and if this frequency can be output by any of the device's pin and if this frequency can be input by any pin of the device. By the way, the project we are working on need the frequency is th...

xzhan.22 by Associate
  • 1499 Views
  • 2 replies
  • 0 kudos

Encoder read error

Hi there!i start to work with a rotary encoder, i configurate a timer 3:in this way and i enable the interrupt . for read the encoder inside the timer interrupt i write nuber= (TIM3->CNT)>>2;so when i read the varible the first time i see 0 - 1- 2- 3...

0693W00000Y93vJQAR.png
SGian.1 by Senior
  • 1734 Views
  • 3 replies
  • 0 kudos

Resolved! Powering STM32 Blue pill through external source via micro USB

Hello, I've a strange problem and I can't find the answer on internet.I'm transmitting a data from UART2 of my STM32 Blue pill. Its just one line :- HAL_UART_Transmit(&huart2, (uint8_t*)Tx_msg, sizeof(Tx_msg), 100);While using with ST-Link, it works....

0693W00000Y9jo0QAB.png
Mshar.2 by Associate II
  • 3777 Views
  • 2 replies
  • 0 kudos

Resolved! SDIO/EMMC version of STM32 versus EMMC IC version

Hi I want to use an EMMC( INSIGNIS NSEC53K) with STM32F405 SDIO interface. STM32F405 manual says: "Full compliance wit MhultiMediaCard System Specification Version 4.2."the EMMCwe have chosen: INSIGNIS NSEC53K. Its datasheet says:"Compliant with eMMC...

MK..1 by Senior
  • 2489 Views
  • 3 replies
  • 0 kudos

How to send 10-bit message using HAL_SPI_TRANSMIT

I am trying to interface with an AD8400 single channel digital potentiometer. It communicates over SPI and requires 2 address bits and 8 data bits to set its resistance. I am having trouble figuring out how to send a 10-bit message.I have set the dat...

0693W00000Y9hW9QAJ.png 0693W00000Y9hW4QAJ.png
PMalh.1 by Associate II
  • 7862 Views
  • 9 replies
  • 0 kudos

ADC reading on STM32H7B0 CPUs

Hi!I am having problems reading accurate values using the STM32H7B0 CPU. I have identical boards with STM32H7A3 and STM32H7B0 CPUs and the results from the B0 boards are off by a lot. I have also tried to run the ADC in 12 vs 16 bit mode and the scal...