2022-08-05 5:20 AM
Dear ST Community,
as part of a project to capture analog microphone data, I would like to use my own callback funtions instead of hal callbacks. For this I register my ADC callbacks with the HAL function HAL_ADC_RegisterCallback as follows:
/*************** ADC Section Begin ********************/
hadc1.Instance = ADC1;
...
hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
/* Register TIM Callbacks */
HAL_ADC_RegisterCallback( &hadc1, HAL_ADC_MSPINIT_CB_ID, Microphone_ADC_MspInit );
HAL_ADC_RegisterCallback( &hadc1, HAL_ADC_MSPDEINIT_CB_ID, Microphone_ADC_MspDeInit );
HAL_ADC_RegisterCallback( &hadc1, HAL_ADC_CONVERSION_COMPLETE_CB_ID, Microphone_ADC_ConvCpltCallback );
HAL_ADC_RegisterCallback( &hadc1, HAL_ADC_CONVERSION_HALF_CB_ID, Microphone_ADC_ConvHalfCpltCallback );
HAL_ADC_RegisterCallback( &hadc1, HAL_ADC_ERROR_CB_ID, Microphone_ADC_ErrorCallback );
status = HAL_ADC_Init( &hadc1 );
if( status != HAL_OK)
{
_SYSTEM_LOG( "HAL_ADC_Init Error Code: [%d]", status );
return status;
}
else
{
/* Everything Okay. Do Nothing */
}If I register all five callbacks right before HAL_ADC_Init(), the Half and Complete are never called.
But if I register the Half + Full Complete callback after HAL_ADC_Init the AD conversion works and all own callbacks are called.
At the moment it is not clear to me in which order I have to register which callback where. (Independently from ADC TIM or other callbacks)
Thank you for the support
Solved! Go to Solution.
2022-08-05 5:39 AM
I figured it out. I'm too stupid to read:
UM1905 ADC Firmware driver API description:
Callbacks can be registered/unregistered in @ref HAL_ADC_STATE_READY state only. Exception done MspInit/ MspDeInit functions that can be registered/unregistered in @ref HAL_ADC_STATE_READY or @ref HAL_ADC_STATE_RESET state, thus registered (user) MspInit/DeInit callbacks can be used during the Init/ DeInit. Then, the user first registers the MspInit/MspDeInit user callbacks using @ref HAL_ADC_RegisterCallback() before calling @ref HAL_ADC_DeInit() or @ref HAL_ADC_Init() function.
2022-08-05 5:39 AM
I figured it out. I'm too stupid to read:
UM1905 ADC Firmware driver API description:
Callbacks can be registered/unregistered in @ref HAL_ADC_STATE_READY state only. Exception done MspInit/ MspDeInit functions that can be registered/unregistered in @ref HAL_ADC_STATE_READY or @ref HAL_ADC_STATE_RESET state, thus registered (user) MspInit/DeInit callbacks can be used during the Init/ DeInit. Then, the user first registers the MspInit/MspDeInit user callbacks using @ref HAL_ADC_RegisterCallback() before calling @ref HAL_ADC_DeInit() or @ref HAL_ADC_Init() function.