Hello everybody!I was wondering if the time of the HAL_SPI_Transmit function can be shorter. (see the picture for more info) ,I use the STM32L031K6 dev. board which runs at 32 MHz with a ARM Cortex -M0+. I set de the baudrate to (/2), which is max, f...