STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32h743 max FMC SDRAM clock 100MHz?

Hi,I found this in datasheet But we config SDRAM at 120MHz, because we are running at 480MHz.(480MHz / 2 / 2 = 120MHz).I am thinking the datasheet is for STM32H7xx 400MHz, because when I config SDRAM at 120MHz, the system works fine without issue.Doe...

_legacyfs_online_stmicro_images_0693W00000bhavNQAQ.png
Dat Tran by Senior II
  • 2757 Views
  • 3 replies
  • 0 kudos

STM32F407VE sector 4 erase problems

I made a mistake a few days ago that resulted in my program erasing part of itself. \\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\I'm doing a bare metal bootloader on a STM32F407VE and ha...

BKuhn by Associate III
  • 2592 Views
  • 4 replies
  • 0 kudos

hcan1 not working while hcan2 does work with same settings

I'm working with a custom STM32F105 board with two similar CAN circuits but CAN1 is not working.I use STM32 HAL with this custom CAN lib which handles configuration and buffering.It was working before with the same hardware but I can't get it woking ...

MEige.1 by Associate III
  • 1699 Views
  • 2 replies
  • 0 kudos