cancel
Showing results for 
Search instead for 
Did you mean: 

I cannot get a Timer Capture to work on STM32F7805-DK

BBrow.2
Associate III

I have tried Timer 2 CH1, and Timer 3 CH1. No Luck.

I know the pin has a square wave going into it and the timer is counting, because I can poll GPIOB->IDR and read TIM3->CNT.

Nothing I can do can get a reading other then zero from TIM3->CC1

I cannot get a IRQ from TIM3 unless I force it via TIM3->EGR |= 2;

My Init Code:-

void InitTimer3(void)

{

GPIOB->PUPDR &= ~(3<<8); // No Pullup or Pulldown

GPIOB->OSPEEDR |= (3<<8); // Very High speed

GPIOB->MODER &= ~(3<<8); // PB4 Input

GPIOB->AFR[0] &= ~(0x0F << 16);

GPIOB->AFR[0] |= (2<<16); // AF2

RCC->APB1ENR |= 2; // Timer 3 enable

RCC->AHB1ENR |= 2; // PORTB Clock Enable

TIM3->CCER = 0;

TIM3->PSC = 511; // Prescale

TIM3->ARR = 0xFFFF;//250; // Max Count

TIM3->CCMR1 = 1; // Compare 1

TIM3->DIER = (1<<1) | 1; // CC1 IRQ enabled

TIM3->CR1 = (1<<7) | 1; // Enabled, UP, Auto Reload Buffered

TIM3->CR2 = 0;

TIM3->CCER = (1<<3) | (1<<1) | 1;//1; // Enable Compare 1, Both Edges

TIM3->SR = 0;

NVIC_SetPriority(TIM3_IRQn, 0);

NVIC_EnableIRQ(TIM3_IRQn);

}

My IRQ:-

void TIM3_IRQHandler(void)

{

if ((TIM3->SR & 2) != 0) // Capture 1

{

Dwell ++;

TIM3->SR &= ~2;

}

if ((TIM3->SR & 1) != 0) // OVF WORKS!!!!!!

{

TIM3->SR &= ~1;

}

}

Dwell will not advance, unless I put Dwell ++; into the OVF code

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
BBrow.2
Associate III

Found it!!!

GPIOB->MODER |= (2<<8); // Alternative Function Mode

So not only do you have to choose the applicable AF via GPIOB->AFR, but also set MODER to AF mode!

*SOLVED*

View solution in original post

4 REPLIES 4
waclawek.jan
Super User

If you enable GPIOB clock *after* you set its registers, then those registers won't get set.

If in doubts, the first thing always is to read out the relevant registers content and check/compare.

JW

PS. Don't

TIM3->SR &= ~2;

do

TIM3->SR = ~2;

BBrow.2
Associate III

Thankyou for your quick response.

I moved the RCC clock enables to the begining of the Init code, and put an ELSE on the OVF IF to see what else is happeneing.

Now some real strange things happen:-

Erratically, I get the OVF ELSE excecuting, which would indicate another IRQ source. Only problem is, that source is not CCR1! When that happens, TIM3->SR reads back as 28 (B2, B3, B4), which are output compares (disabled) and they do not have the ability to generate an IRQ with this code!

Still no IRQ from CCR1.

Does that make sense? After Init, All registers read back correct.

Also, I need to use TIM3->SR &= ~2 to clear ONLY bit 1. Without the & it will clear all other IRQ flags as well. I want to preserve the other flags.

BBrow.2
Associate III

So My new code:-

void InitTimer3(void)

{

RCC->APB1ENR |= 2; // Timer 3 enable

RCC->AHB1ENR |= 2; // PORTB Clock Enable

GPIOB->PUPDR &= ~(3<<8); // No Pullup or Pulldown

GPIOB->OSPEEDR |= (3<<8); // Very High speed

GPIOB->MODER &= ~(3<<8); // PB4 Input

GPIOB->AFR[0] &= ~(0x0F << 16);

GPIOB->AFR[0] |= (2<<16); // AF2

TIM3->CCER = 0; // Timer Channel OFF

TIM3->PSC = 511; // Prescale

TIM3->ARR = 0xFFFF; // Max Count

TIM3->CR1 = (1<<7) | 1; // Enabled, UP, Auto Reload Buffered

TIM3->CR2 = 0;

TIM3->CCMR1 = 0; // Clear

TIM3->CCMR1 |= 1; // Compare 1

TIM3->CCMR1 |= (3<<4); // Filter

TIM3->CCER = 10; // Capture on both edges

TIM3->CCER |= 1; // Enable Compare 1

TIM3->DIER |= 3; // CC1 + TOF IRQ enabled

NVIC_SetPriority(TIM3_IRQn, 0);

NVIC_EnableIRQ(TIM3_IRQn);

}

//

//

//

void TIM3_IRQHandler(void)

{

if ((TIM3->SR & 1) != 0) // OVF

{

TIM3->SR &= ~1;

Dwell ++;

}

else

Debug+= 100;

if ((TIM3->SR & 2) != 0) // Capture 1

{

Debug++;

TIM3->SR &= ~2;

}

Dwell ++;

}

SO if Dwell is not an even number, then an IRQ other then TOF Update has occured. It is always Even.

Debug always stays on ZERO, so no CCR1 IRQ.

BBrow.2
Associate III

Found it!!!

GPIOB->MODER |= (2<<8); // Alternative Function Mode

So not only do you have to choose the applicable AF via GPIOB->AFR, but also set MODER to AF mode!

*SOLVED*