STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Problem with Flash write STM32G474RE

Dear colleagues,I woild like to ask you help me with may issue below:Why do I lose data when writing flash memory and an error occurs my code in the attachment.Code seems good, but I am sure that I loose something.In memory loosed letters "llo" from ...

IPast.1 by Associate II
  • 5421 Views
  • 6 replies
  • 0 kudos

Resolved! STM32驱动EC11编�?器

使用STM32F446RE的Tim encode模�?接�?�EC11编�?器数�?��?�以区分正�??转�?�?如何使用LL库实现?

YLi.13 by Associate II
  • 2542 Views
  • 6 replies
  • 0 kudos

FMC vs FSMC

Hello,A product I'm working on requires communicating with an FPGA over an 8 bit data + 24 bit address bus.To support a legacy design with the least possible changes I need the bus to toggle at 43.75 MHz.All I need is single (non-burst) address acces...

skon.1 by Senior
  • 5305 Views
  • 3 replies
  • 0 kudos

Resolved! stm32f446re gpio as active LOW reset pin

im using pc8 as a reset pin and ive check it with a logic analyzer and wen its initalized it drops low then goes back to high before im calling my function to drop it low btw im using saleae logic 2 void reset_pin_init(void){ //PC8 RCC->AHB1ENR |= ...

Cannot find a single STM32H7 series chip at any of the standard sellers in North America while the STM32MP series can be found anywhere, so my question is;What does support, in terms of manufacturing, of the STM32H7 look like in the future?

I refuse to purchase a $40 chip for over $400 dollars so will not purchase on current market. I based an entire product line on the STM32H757 and now I cannot buy them so the real question is, should I move to a different processor?

rwareinc by Associate III
  • 5533 Views
  • 11 replies
  • 0 kudos

Resolved! Implementing w5500 to stm32l431rct6

Hi everyoneI'm a student and I'm totally new to stm32 controllersI spend two weeks trying connecting stm32l431rct6 to w5500 but I failedcan any one guide me to a tutorial or some videos that I can use ? or can anyone help methank you

Abdegou_8 by Associate II
  • 5386 Views
  • 2 replies
  • 0 kudos