DMA - update timer pwm dutyCycle is working but if dma overflow back to 0 there are no values written
I expect from DMA, squence 1000,0010,0100,0001
but I get out of my timer outputs:
1000,0010,0100,0001,0000
how to remove last "0000"
my code is:
main.c
extern DMA_HandleTypeDef hdma_tim1_ch1;
extern DMA_HandleTypeDef hdma_tim1_ch2;
extern DMA_HandleTypeDef hdma_tim1_ch3;
extern DMA_HandleTypeDef hdma_tim1_ch4_trig_com;
uint16_t speed = 10;
uint16_t speednew = 10;
uint16_t speed2;
uint16_t power;
uint16_t pwmss1[4];
uint16_t pwmss2[4];
uint16_t pwmss3[4];
uint16_t pwmss4[4];
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_TIM1_Init(void);
static void MX_ADC1_Init(void);
static void MX_TIM3_Init(void);
int16_t out1;
int16_t out2;
int16_t out3;
int16_t out4;
pwmss1[0] = 1000;
pwmss1[1] = 0;
pwmss1[2] = 0;
pwmss1[3] = 0;
pwmss2[0] = 0;
pwmss2[1] = 0;
pwmss2[2] = 1000;
pwmss2[3] = 0;
pwmss3[0] = 0;
pwmss3[1] = 1000;
pwmss3[2] = 0;
pwmss3[3] = 0;
pwmss4[0] = 0;
pwmss4[1] = 0;
pwmss4[2] = 0;
pwmss4[3] = 1000;
HAL_TIM_PWM_Start_DMA(&htim1, TIM_CHANNEL_1, (uint32_t *)pwmss1, 4);
HAL_TIM_PWM_Start_DMA(&htim1, TIM_CHANNEL_2, (uint32_t *)pwmss2, 4);
HAL_TIM_PWM_Start_DMA(&htim1, TIM_CHANNEL_3, (uint32_t *)pwmss3, 4);
HAL_TIM_PWM_Start_DMA(&htim1, TIM_CHANNEL_4, (uint32_t *)pwmss4, 4);
speed2 =65000;
power = 0;
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
TIM3->CCR4 = power;
TIM1->PSC = speed2;
out1 = HAL_GPIO_ReadPin(GPIOA, GPIO_PIN_8);
out2 =HAL_GPIO_ReadPin(GPIOA, GPIO_PIN_9);
out3 =HAL_GPIO_ReadPin(GPIOA, GPIO_PIN_10);
out4 =HAL_GPIO_ReadPin(GPIOA, GPIO_PIN_11);
}
}
/**
* @brief System Clock Configuration
* @retval None
*/
static void MX_TIM1_Init(void)
{
/* USER CODE BEGIN TIM1_Init 0 */
/* USER CODE END TIM1_Init 0 */
TIM_MasterConfigTypeDef sMasterConfig = {0};
TIM_OC_InitTypeDef sConfigOC = {0};
TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig = {0};
/* USER CODE BEGIN TIM1_Init 1 */
/* USER CODE END TIM1_Init 1 */
htim1.Instance = TIM1;
htim1.Init.Prescaler = 720;
htim1.Init.CounterMode = TIM_COUNTERMODE_UP;
htim1.Init.Period = 1000;
htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim1.Init.RepetitionCounter = 0;
htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;
if (HAL_TIM_PWM_Init(&htim1) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;//updated was reset
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
sConfigOC.OCMode = TIM_OCMODE_PWM1;
sConfigOC.Pulse = 0;
sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
sConfigOC.OCNPolarity = TIM_OCNPOLARITY_HIGH;
sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
sConfigOC.OCIdleState = TIM_OCIDLESTATE_RESET;
sConfigOC.OCNIdleState = TIM_OCNIDLESTATE_RESET;
if (HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_2) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_3) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_4) != HAL_OK)
{
Error_Handler();
}
sBreakDeadTimeConfig.OffStateRunMode = TIM_OSSR_DISABLE;
sBreakDeadTimeConfig.OffStateIDLEMode = TIM_OSSI_DISABLE;
sBreakDeadTimeConfig.LockLevel = TIM_LOCKLEVEL_OFF;
sBreakDeadTimeConfig.DeadTime = 0;
sBreakDeadTimeConfig.BreakState = TIM_BREAK_DISABLE;
sBreakDeadTimeConfig.BreakPolarity = TIM_BREAKPOLARITY_HIGH;
sBreakDeadTimeConfig.AutomaticOutput = TIM_AUTOMATICOUTPUT_DISABLE;
if (HAL_TIMEx_ConfigBreakDeadTime(&htim1, &sBreakDeadTimeConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN TIM1_Init 2 */
/* USER CODE END TIM1_Init 2 */
HAL_TIM_MspPostInit(&htim1);
}
/**
* Enable DMA controller clock
*/
static void MX_DMA_Init(void)
{
/* DMA controller clock enable */
__HAL_RCC_DMA2_CLK_ENABLE();
/* DMA interrupt init */
/* DMA2_Stream1_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA2_Stream1_IRQn, 1, 0);
HAL_NVIC_EnableIRQ(DMA2_Stream1_IRQn);
/* DMA2_Stream2_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA2_Stream2_IRQn, 1, 0);
HAL_NVIC_EnableIRQ(DMA2_Stream2_IRQn);
/* DMA2_Stream4_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA2_Stream4_IRQn, 1, 0);
HAL_NVIC_EnableIRQ(DMA2_Stream4_IRQn);
/* DMA2_Stream6_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA2_Stream6_IRQn, 1, 0);
HAL_NVIC_EnableIRQ(DMA2_Stream6_IRQn);
}