STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Need Tray dimension MPN-STM32F412ZGT6

Hi Expert,Good day.STM32F412ZGT6 are come in Reel packaging, I need the tray dimensions to ensure the tray fits properly in the pick-and-place machine. What is the feeding direction and pitch dimension? Could you help me locate the tray drawings for ...

Resolved! STM32 N6 FSBL USART doesn't work

Hi, I have been trying to study how to use the N657X0 Nulceo board. When I tried to test the USART of the board with an FSBL project, there was no print on the serial monitor, and I could not find the reason. Could somebody check what the problem is ...

HANITALY by Associate III
  • 262 Views
  • 1 replies
  • 0 kudos

Resolved! Milliseconds Deviations in toggling led for one second

Hi,I have been using Tim11 general purpose timer in Nucleo-f410rb micro controller board to blink an led at a delay of 1 second but there is a deviation of 18 ms in it. which have a 16 bit prescaler and 16 bit auto reload counter with it. In the .ioc...

ioc file for forum.png Screenshot from 2025-05-26 16-39-08.png

Resolved! Question about STM32 H7 Series Function

[Inquiry Regarding Large-Scale Library Operation on STM32H7-Based System] MCU: STM32H7 Series (Planned) OS: FreeRTOS Memory Configuration: External SDRAM External Serial Flash (QSPI) Our company is planning to utilize large-scale libraries. We...

ishwang by Associate
  • 389 Views
  • 1 replies
  • 0 kudos

SIL2/SIL3

Hi!May I ask the relevant safety experts from ST, I have now applied for the STEVAL-SILKT01 development board from ST Company and have signed the NDA. Are there any demo examples related to the STEVAL-SILKT01 development board? If so, could you provi...

HomeLand by Associate
  • 227 Views
  • 1 replies
  • 0 kudos

STM32G4 HRTIM burst mode enable / disable

In the reference manual for the G474, under HRTIM Burst mode control register (HRTIM_BMCR), bit 31 is the BMSTAT register; it gives the current operating status of the burst mode feature. But it states that writing this bit to zero causes early burst...

Jbin0101 by Associate II
  • 394 Views
  • 1 replies
  • 0 kudos