STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

GPIO toggle in interrupt timer

I'm trying to create a Synchronous communication using a timer and GPIO.I can toggle a pin-up to 1Mhz inside the main function, but if I try to toggle gpio inside the timer interrupt handler, the max toggle speed is around 300khz. Is there a reason f...

Pacioc193 by Associate II
  • 3426 Views
  • 4 replies
  • 0 kudos

Resolved! ADC DMA not restarting after exiting STOP mode

Hello!I have my ADC DMA setup so that Timer 1 will trigger a conversion with a specific frequency. Both DMA continuous requests and Continuous conversions are disabled. DMA is set to Normal mode.When the buffer is full and HAL_ADC_ConvCpltCallback is...

BZhou.2 by Associate
  • 2671 Views
  • 1 replies
  • 0 kudos

Resolved! STM32L0X0 Series - No UART Half Transfer Flag/Bit Documented?

Unless I'm missing something, I don't see a HT flag documented in the STM32L0X0 reference manual in the USART_ISR register. I see the TC, idle, etc. flags. So how is that interrupt getting triggered (because I have verified it does get triggered)? ED...

nobbyv77 by Associate II
  • 1727 Views
  • 2 replies
  • 0 kudos

STM32G030K6T6 - Rtc with sub second

HiI would like to use the sub second information available in the rtc registers. Can some one give an exemple on how to use it correctly with HAL?BRGilberto

GErma.1 by Associate III
  • 2010 Views
  • 3 replies
  • 0 kudos

Why is my PIN configured as Input, but still acts as Output?

Hi allI'm working on Nucleo-F410RBI have a UV filter that sends back a 0V-5V digital signal that I'm trying to read on PIN D13 (PA5).The issue if the following (I'm using a multimeter to read the voltage, and all components have a common ground):when...

_legacyfs_online_stmicro_images_0693W00000bj4sKQAQ.png
Dali by Associate
  • 1615 Views
  • 2 replies
  • 0 kudos