STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Disabling the pull-down on PB6 (UCPD1_CC1) via PA9

Hello,we currently have a problem using PB6 of an STM32G474ME as FDCAN-TX: During Reset, it is pulled down to GND, which we attribute to the USB-C functionality. This causes the FDCAN-TX line to send a dominant signal during reset of the STM32.As per...

BGott.1 by Associate
  • 1312 Views
  • 1 replies
  • 0 kudos

Resolved! RCC configuration results in HardFault (STM32F411CEU6).

I have a board that is running well. There are about 50+ PCBs in production operating fine. The firmware is pretty complex, but the hardware relatively simple, just some SPI devices and some PWM outputs.I revved the board, and the new board doesn't w...

YvanR by Associate II
  • 3536 Views
  • 3 replies
  • 0 kudos

Custom linker section with fixed offset address

Hi!I'd like to set a custom section in the linker script file to store firmware specific constant data. This section should be at the head of the firmware binary with a fix offset address. I was able to create a section at the end of flash area but t...

GPIO toggle in interrupt timer

I'm trying to create a Synchronous communication using a timer and GPIO.I can toggle a pin-up to 1Mhz inside the main function, but if I try to toggle gpio inside the timer interrupt handler, the max toggle speed is around 300khz. Is there a reason f...

Pacioc193 by Associate II
  • 3378 Views
  • 4 replies
  • 0 kudos