STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STEPPER MOTOR using I2C

Hi, I have a problem with starting a stepper motor using the I2C bus. It uses the NUCLEO-F746ZG microprocessor, the SMC 64-BP stepper motor driver and the KH1634-03CA stepper motor. The main problem is finding the address of the controller and giving...

PBiał.1 by Associate II
  • 3821 Views
  • 2 replies
  • 0 kudos

How to reduce the consumption of the Nucleo-L073RZ board to less than 700uA? How to disable J-Link part on the board?

I am developing a card with a supercap storage, I designed it for a consumption of 40uA as it is written in the datasheet, however I reach only 3mA and I use the "standby" mode written and found on the internet. Can you explain me how to disable the ...

Thomcheh by Associate
  • 1960 Views
  • 2 replies
  • 1 kudos

Resolved! Hi..I am using STM32U575 NUCLEO ..there are three drive levels are mentioned for LSE...which one one should be used or which is more suitable for low power consumption and I need to know the power consumption in each case (numerical value)..

In the errata sheet,it is mentioned that low drive mode and medium low drive are not working.. but I checked and they work fine...is there any correction in the errata sheet...?..Can I go with low drive mode for LSE (NUCLEO-U575ZQ)???

ABDUL1 by Associate II
  • 4256 Views
  • 8 replies
  • 0 kudos

How should I study STM32 MCU

Hello,I am a mechanical engineer that is studying Mechatronics as master degree. I am getting keen on embedded system after I have taken a course on operating systems on embedded systems. I have never used STM32 word and I have just received a stm32f...

DAlta.1 by Associate II
  • 2030 Views
  • 3 replies
  • 0 kudos

Resolved! STM32U585AII6QU and STM32U5A5AJ Obsolesce status for the controller, How long min and max years this controller will be there in Market?

Hi, We are CYIENT technologies focused on Engineering, manufacturing, Data Analytics, Operational and Networking.we are using STM32 controller and other ST components in one of our projects. And our Product will be active 8 years in market. I would l...

Madhu by Associate
  • 1486 Views
  • 2 replies
  • 0 kudos