STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32G473VCT Internal voltage reference setup failing

Hi All,I created an STM32CubeIDE project to set up an Internal voltage reference on myboard that has an STM32G473VCT; see the screenshot attached. All I did wascreate that Internal voltage reference, save and generate code. See screenshot: I put brea...

_legacyfs_online_stmicro_images_0693W00000bkJPBQA2.png
IAuto.1 by Associate II
  • 2603 Views
  • 4 replies
  • 0 kudos

How to use COMP on STM32g431c8T6? I found it not work correctly. The pol is noninverted When INP(1.6V)<INM(2v),the out is high. Only INP=0, the out is low.

void Comp1Init(void){ Comp1GpioInit(); RCC -> APB2ENR |= 1;  //20230506///////////////////////////////////////////////////////// COMP1 -> CSR |= 3 << 19;//TIM3 OC3 Banking of CSA p739 /////////////////////////////////////////////////////////// COMP1 ...

立张.1 by Associate II
  • 941 Views
  • 0 replies
  • 0 kudos

Resolved! Unique fw for 2 ST MCU

Hi... we are deciding if has a sense to develop a electronic board able to host to different mcus (STF4 and STH5) and giving an external hw trigger the unique fw should be able to run the part relevant to F4 series or H5 series. The question is how m...

SGasp.1 by Senior
  • 1514 Views
  • 2 replies
  • 0 kudos

Resolved! STML433 ADC1 coexist with other GPIO

Hi,I working with STM32L433's ADC, and I'm having a problem where the ADC CH11 couldn't coexist with other GPIOs. I'm using a resistor divider from a battery and feeding into ADC1 CH11 (PA6, pin16). If the PA5 is left in a reset state, it all works. ...

_legacyfs_online_stmicro_images_0693W00000bkL9JQAU.png _legacyfs_online_stmicro_images_0693W00000bkL9dQAE.png
YKuo.1 by Associate II
  • 2080 Views
  • 3 replies
  • 0 kudos