Skip to main content
mkilicaslan
Visitor II
January 16, 2023
Question

Hardware reset need after programming to lower current consumption.

  • January 16, 2023
  • 1 reply
  • 1200 views

When I program to my stm32 MCU, I need to hard reset to lower the current consumption. I mean, after I programmed the MCU, the board consume 580uA. Then I do a software reset via NRST and still had the same current consumption. Then I do a hard reset (GND-VCC short), and the current consumption drops to 6uA. Why do I need a hardware reset? By the way, the code enters STOP2 mode.

This topic has been closed for replies.

1 reply

MM..1
Super User
January 16, 2023

1- this is named power down reset

2- if you programm mcu with config debug in low power mode enebled = STOP2 isnt real disable it

3- this all is controll by MCUDBGREGS , that isnt reset with NRST only with power off or prog in code