FW upgrade via DFU
I am trying to upgrade my uC via dfu-util however i receive an error and i do not know how could i debug it dfu-util: Error during download get_status
dfu-util 0.9
Opening DFU capable USB device...
ID 0483:df11
Run-time device DFU version 011a
Claiming USB DFU Interface...
Setting Alternate Setting #0 ...
Determining device status: state = dfuIDLE, status = 0
dfuIDLE, continuing
DFU mode device DFU version 011a
Device returned transfer size 1024
DfuSe interface name: "Internal Flash "
Downloading to address = 0x08000000, size = 638548
Download [=========================] 100% 638548 bytes
Download done.
File downloaded successfully
dfu-util: Error during download get_status