STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

One pulse mode configuration

Hello to everyone,I would like to know more about 'one pulse mode'. I'm using a STM32F446RET and I need to generate 1 or more pulses when an event occours.In my project, channel 1 of TIM9 is the pin chosen to generate the waveforms.I got that the 'on...

Las1_0-1687944025035.png
Las1 by Associate II
  • 14361 Views
  • 9 replies
  • 1 kudos

Resolved! Critical issue with I2C and DMA on new STM32U5

I experience a strange problem with I2C, DMA and the latest STM32U575ZI-Q, not seen on L4 and H7 MCUs.After a successful data transfer from SMBus target (slave) to controller (host) the last PEC byte stays in RXDR registry. On the next transfer in th...

TDJ by Lead
  • 2639 Views
  • 2 replies
  • 0 kudos

STM32F04 USB

Hi everyone!I am building a portable device wich has a batery, obviusly, and the MCU is the STM32F042. I need to use an USB to program it and charge the batery. Anyone can provide me with any schematic that I can use for the USB conections?Thank you.

Resolved! FDCAN2 doesn't seem to work with STM32G474e-EVAL board

I'm having problems getting my software to work with FDCAN2 on the STM32G474e-EVAL board. It works with FDCAN1, but w/ FDCAN2, messages accumulate in the Tx buffer until I get buffer fill errors.I built the FDCAN_Com_IT example from the latest STM32G...

ESchn.1 by Associate II
  • 6093 Views
  • 11 replies
  • 1 kudos

Resolved! SRAM2 erased on backup domain reset

Hi @all,we have an application, where we use the LSE. In due to weaknesses of the part we use, the LSE can fail sometimes.If I then use the __HAL_RCC_BACKUPRESET_FORCE() and __HAL_RCC_BACKUPRESET_RELEASE() to reset the LSE and LSI system, also the SR...

PScal by Associate III
  • 11293 Views
  • 10 replies
  • 7 kudos

Using USB-DFU bootloader mode

Is it necessary to enable and define the USB-port in CubeMX in order to be able to use the USB-DFU bootloader mode? And if so, what should the settings be for the STM32F415?

RHarte by Associate II
  • 847 Views
  • 0 replies
  • 0 kudos

stm32f407 protection level 2

Hello. I have set protection level 2 in stm32f407. Now I need to change the project a little bit, but st-link/v2 can't connect to the target. How will I able to reset level 2 and do 'mass erase' that chip?Thanks.

BIgor by Associate
  • 2089 Views
  • 1 replies
  • 0 kudos