STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STUSB1600 Source Role Comunication USB 2.0

I project a board for my company based on STUSB1600 for the part of Power Delivery with a USB Type-C port where I want to connect a device.Before sending the board into production, I purchased the evaluation board STEVAL-CCC002V1 to conduct tests wit...

CAN auto retransmission enabled

hello,i have enabled the Automatic retransmission and sending data on TX. There is no other node is connected, so there is NACK on sending data. but I see not complete data is transmitted in further attempts. please see attached file and let know wha...

Nico3 by Senior
  • 1657 Views
  • 0 replies
  • 0 kudos

I2C error recovery

Posted on August 24, 2013 at 12:05Hello,I'm trying to make the STM32L152  I2C communication failure-proof against glitches/short-circuits. There's an API command I2C_SoftwareResetCmd which seems to be the cure, but i can't find any proper example or...

Resolved! Unable to use UART over USB on STM32F051 Discovery board

Hello all,I am trying to send "Hello World" to my computer through using the guide below but nothing is sending to the port. I cant see anything on Tera Term. (https://wiki.st.com/stm32mcu/wiki/STM32StepByStep:Step3_Introduction_to_the_UART) (of cour...

Cannot get PWM to work on the STM32L552-Q board

I have turned on the Timer 1 and have gone through several tutorials to get pins PE0, PE11, PE13 and PE14 to pulse but I cannot get any sort of signal output. I'm attaching to project.  The configurations are in main.h, I turn all the timers on in Ma...

wfd by Associate II
  • 4624 Views
  • 5 replies
  • 0 kudos

Resolved! STM32F767 Change RDP level from second stage bootloader

Hello,I have second stage bootloader in place and want to change RDP level from it (0 to 1 and roll back when doing firmware upgrade).However, the problem is, once RDP level is changed to 1, bootloader is not able to change it back to 0. I've to chan...

SGAUR.1 by Associate III
  • 5827 Views
  • 9 replies
  • 6 kudos

Resolved! SPI TXE flag set early

Hi,I m testing SPI TXE flag with the following code:void TestSPI(void){ GPIO_ResetBits(GPIOA, GPIO_Pin_4); SPI_I2S_SendData(SPI3, 0); while (!SPI_I2S_GetFlagStatus(SPI3, SPI_I2S_FLAG_TXE)); SPI_I2S_SendData(SPI3, 0); while (!SPI_I2S_Ge...

SebB by Associate II
  • 4140 Views
  • 5 replies
  • 2 kudos