STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32G0: PWM Generation

I am using NUCLEO-G071RB. I am trying to generate an PWM pulse. I am using TIMER 3 Channel 2. - Clock Frequency = 64 MHzWith this setting I should get a HIGH pulse of 90 micro second, instead I get 80 or 40 micro seconds. When the Pre-scaler is incre...

jowakar122_0-1761917837043.png

USBX mic streaming on WBA65

Hello ST Community,I'm working on implementing USB Audio Class 2.0 with both speaker and microphone functionality on STM32WBA65 using USBX middleware.Request for Example: Are there any complete working examples of USBX Audio Class 2.0 with microphone...

In Windows I can't see USBD Descriptors

 Hello there, I use USB CDC interface and I am sure that all my configurations are okey. There is no problem about connecting and data transfer between windows and my system, but there is a problem about descriptors such as "Manufacturer" or name of ...

Durukan by Associate
  • 1875 Views
  • 4 replies
  • 3 kudos

Resolved! Power Supply for STM32F030 Cortex TSSOP20 VDDA and VDD pin

Please i need help. The datasheet, says the VDDA voltage level must be always greater or equal to the VDD voltage leveland must be provided first. My qustion is: will my circuit work, if I tie the VDDA and VDD together, to be powered by the same  LDO...

fredy by Associate
  • 1016 Views
  • 5 replies
  • 3 kudos

Bare metal USART2 clock speed question

Hello,I am learning bare metal programming for STM32F446RE and am trying to write a simple transmit driver for USART2. I managed to do it but my only problem is when I use HSI 16Mhz clock speed (or anything lower) I get a weird first character. When ...

STMnoob_0-1758935979151.png
STMnoob by Associate II
  • 1172 Views
  • 6 replies
  • 2 kudos

Resolved! About FDCAN ERROR

Dear STM experts:     I am using the STM32G473RET6 chip for classic mode communication debugging in FDCAN, but there is a phenomenon where I cannot send information. In FDCAN-PSR, I can see an error of LEC being 5. After removing the CAN chip (SN65HV...

Resolved! SWD connection failed multiple times on STM32H725

We have a batch of custom boards using the STM32H725IGK3 and have experienced several failures getting started with them as the SWD interface appears to be fried. Initially we thought just bad luck with the first couple (inexperienced engineers or ?)...

niallp by Associate III
  • 1686 Views
  • 9 replies
  • 7 kudos

Resolved! GPIO input external pullup question

Testing a board with STM32U5A5. VDD is 3.3VI have configured one GPIO as input with an external pullup to 3.3V through a 470k ohm resistor.The input reads high, but when I measure the input with a scope, I read 2.2V on the input, which is below 0.7VD...

TLin.5 by Associate III
  • 1319 Views
  • 8 replies
  • 4 kudos