User Activity

Hello to alli have build my project as programmer on stm32f103c8t6 to connect as master host to slave one stm32f103c8t6 and program the slave device with code which saved in eeprom connected to the master with i2c it working well with me but I need t...
HELLO TO ALLI HAVE A PROBLEM WHEN I BUILD THE CODE AND PROGRAM IT WITH STM32 PROGRAMMER IT IS WORKING BUT WHEN I TRY TO DOWNLOAD THE CODE USING THE IDE WITH DEBUG I GOT ERR  THIS IS THE CONCOL LOG     ST-LINK SN : 310009000B00004C3359534EST-LINK FW :...
hello to alli want to build project on bluepill board i want to include stm32-mw-openbli got it from https://github.com/STMicroelectronics/stm32-mw-openbl  is there any example for thishaw to include in ide
hello to alli want to build project with 2 blue pill firist one have an eeprom it save the file on it the firist blue pill will be as programmer to program the file from the eeprom on the secound blue pill the secound one will be as slavei want to pr...