STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32 i2c transmitter mode flags doubt

why need to monitor txe flag and btf flag to transfer data after each byte.txe says data register is empty,btf  and txe says need monitor after last byte. according to reference manual.but my question is how should i know i get ack after sending 1 by...

STM32F302VCT6 - PC14 -> RTC_OUT_CALIB ?

I would like to set a 1Hz signal on the PC14 (RTC_OUT_CALIB). I have found a manual in document AN3371 (see picture in appendix). The code is also in the appendix. Unfortunately, nothing happens on the PC14 but the RTC works. If anyone has any idea w...

_legacyfs_online_stmicro_images_0693W00000dDc1sQAC.png
SimonFu by Associate
  • 379 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H7 DMA

HelloCan the STM32H743 modify data at two non-consecutive peripheral addresses in a single DMA event,A DMA event changes two peripheral addresses,

zhaowhong by Associate III
  • 490 Views
  • 1 replies
  • 0 kudos

Resolved! STM32N6 IMX219 camera

Hello,I'm trying to port the ST IMX335 camera driver middleware to work with the RPi 2 IMX219. Everything works well with the IMX335, however after adjusting to reflect the IMX219 registers I get no image data and a Lane 0& 1 control error flag as so...

Scheduling timers for motor control

Hi!I'm struggling to wrap my head around timers - I am trying to schedule some ADC reads of a current sense amplifier in a motor control setup.I have three center-aligned PWM waveforms being generated by Timer1, which successfully commutate a BLDC mo...

sb_st by Senior II
  • 650 Views
  • 3 replies
  • 0 kudos