User Activity

Hello, I have a few questions on STM32N6 capabilities for USB after reading AN4879, AN5967 and RM0486 documents: 1. AN4879 states that to be compliant with the USB 2.0 FS electrical spec, the DP+ pin must be pulled high. Does this also hold true for ...
In the schematic for STM32N6 Vddcore power rail (attached), voltages of 0.81V and 0.89V are output from the SMPS using resistor dividers. I understand how the output of 0.81V was achieved using the 56K and 160K resistors and formula from the SMPS dat...
I'm following along AN6000 to bypass the internal SMPS of the STM32N6 and use my own SMPS and LDOs power several of the power rails for the MCU and have some questions:1. In section 3.2 "System power/up/uncontrolled power-down sequence", the document...
Hello,I'm reading the article on "How to create an STM32N6 FSBL load and run" and have a couple of questions about DFU implementation on the STM32N6:1. Is DFU possible with the application as part of the FSBL?2. Is there an example on how to implemen...
Kudos from
Kudos given to