STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 with ETM TRACE

Hello,Is there anyone who worked with TRACE ? I use j-trace with stm32h743 and IAR.On testing the trace with SEGGER cortex-m reference board (stm32h7407, which comes with the j-trace product) and IAR, the functionality works great.I then moved to stm...

ranran by Senior II
  • 1699 Views
  • 1 replies
  • 1 kudos

Resolved! Confusion about the size of uncontigous flash

Hello, I am writing about my confusion in "STM32H742, STM32H743/753 and STM32H750 Value line advanced Arm®-based 32-bit MCUs". According to reference manual;STM32H743xI has 2 banks of 1 MByte each forming a contiguous flash memory area, so there woul...

G_A. by Associate II
  • 3938 Views
  • 5 replies
  • 0 kudos

Resolved! STSPIN32G4 with motor voltage of 6V

I want to use the STSPIN32G4 for an application with a motor voltage of 6-8V.  Has anyone ever ran with this low of a motor voltage. The specifications list the minimum motor voltage of 5.5V, so I believe it should be possible.  However, the lowest b...

jcysyk by Associate II
  • 2739 Views
  • 5 replies
  • 1 kudos

Resolved! Correct way to read timer counter register

i have a question regarding the correct way of reading the timer counter registers.I learned not to read timer couter registers asynchronously, because it can lead to spourious wrong values if i read just when the timer changes it's value.In several ...

STM32H743 reference manual FDCAN_NBTP description

Hi,depend on reference manual RM0433 Rev 8 for STM32H743 p.56.5.7 "FDCAN nominal bit timing and prescaler register" the CAN bit time can be programmed max. 81 time quanta. Is documentation correct on this place?Due to described time quantum range [1....

EMonj.1 by Associate II
  • 2212 Views
  • 3 replies
  • 0 kudos

Bit alingment

Hi everyoneI have a problem with a data structure I really want to use, because I would heavenly benefit from the easy access, that it would provide. /* * myTypes.h * * Created on: 02.05.2023 * Author: */ #ifndef INC_MYTYPES_H_ #define I...

Rundumeli by Associate II
  • 2317 Views
  • 3 replies
  • 0 kudos

master full spi register with stm32l010c6t6

Hi everyone! i am work with stm32l010c6t6 for comunicate llcc68 Lora module using spi, i find the standard peripheral library and not have, i don´t want use hal because i need maior control. i am using the example but this is using stm32f103c8t6 and ...

jdo by Associate II
  • 950 Views
  • 0 replies
  • 0 kudos

Resolved! HAL_UART_Receive_IT() only fires once, and I don't know why.

Hi!I am trying to write a program where I am waiting for receiving 6 bytes of data through UART. It works just fine the first time, than I restart the receive_IT function and nothing happens anymore. I have other codes where I use it just the same, t...

BBara.1 by Associate II
  • 12858 Views
  • 11 replies
  • 2 kudos

Where to find DFU examples?

Hello, I have both the B-G474E-DPOW1 and the STM32F407G-DISC1.According to the AN3156 I saw that both the G4 and F4 series support DFU. I wanted to demo this capability with either of these boards, but I can't find any examples specific to these targ...

ewilliams by Associate II
  • 1355 Views
  • 1 replies
  • 0 kudos

NUCLEO-PGEEZ1 on STM32L4R5

Hi,my problem is somehow close to this post "How to run NUCLEO-PGEEZ1 on NUCLEO-L476RG board? " So, I have followed the structure for my board STM32L4R5 IT6 and I don't have error in my program.My problem is, I can't get  my expected result from EEPR...

Screenshot Result.png app_x-cube-eeprma1.png LogicAnalyzer.png
N.goli by Associate
  • 766 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.